MX8 DSI OLED1 touch support on imx8qxp mek (Yocto)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8 DSI OLED1 touch support on imx8qxp mek (Yocto)

1,057 Views
emmett_milliken
Contributor I

I have been working with the iMX8 QuadXPlus MEK with two of the NXP MX8 DSI OLED1 screens attached, and I can't get the touch to work. I followed the instructions in the i.MX Yocto Project User's Guide, and I am able to build an image where the display is working, but touch is not. I am working with 4.14.78_1.0.0_ga and using fsl-imx8qxp-mek-dsi-rm67191 for the device tree. In trying to figure the issue out I found a similar question:

https://community.nxp.com/message/1035302 

but the answer there did not fix the issue. I have the kernel configuration options the same as that post, but the there is no synaptics section of the dts. From what I can tell, this touch screen uses I2C, and none of the I2C devices in the device tree seem to be touch screen related. 

Is there a device tree for this board which does support the MX8 DSI OLED1 with touch?

If not, what all do I need to do to add touch support to fsl-imx8qxp-mek-dsi-rm67191?

1 Reply

772 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Emmett,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE. Just as reference, you could take a look to the following Community threads:

https://community.nxp.com/thread/497477 
 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply