All, I'm working with MX6Q gigabit ethernet design issue, refer to FSL Sabra board, we have designed customer board with AR8031 for gigabit ethernet, but we found ethernet can work at 10/100M stably, but the board cann't work at gigabit ethernet, which can recognize G-bit rounter, but can't build up the communication, can anyone help it? thx
Jack
解決済! 解決策の投稿を見る。
Ethernet cannot function at 1 Gbps. Please refer to the errata doc IMX6DQCE which states that there is a limitation of ENET throughput to around 400 Mbps in an optimized environment.
Ethernet cannot function at 1 Gbps. Please refer to the errata doc IMX6DQCE which states that there is a limitation of ENET throughput to around 400 Mbps in an optimized environment.
David, thx for reply. What we meet is MX6Q Gigabit Ethernet can't work normally via G-rounter, but 10/100M ethernet function can work . I'm not sure whethere someone has the similar experience, thanks.
Jack
Hi Alexander,
I have meet t the similar experience,MX6Q Gigabit Ethernet can't work normally via G-rounter, but 10/100M ethernet function can work,I also do not known what should I do?
What should you do that later? Are you solve this ploblem?
Hi Mrleo,
We have been waiting for a long time, but Freescale hasn't provided solultion. Finally, we have to re-layout our board, and move Ethernet Phy close to MX6Q to solve it. I have inquired Atheros AE team, they said this might be caused by MX6Q, I'm not sure whether Freescale have investiaged this issue by now.
Thx
Jack
Hi,Alexander
You have move freescale Ethernet Phy,what ethernet phy you use can solve this problem?
Thanks,
Leo
P.S, Qualcomm suggest us modify RX_CLK delay and GTX_CLK Delay of AR8031 to enhance system compatibility, but we don't know where to change it, does anyone know it? thanks
Jack
On Freescale website, I haven't found the document about Gigabit ethernet design for MX6Q, does anyone has it? thx.
Jack