Hi All,
I am using MX6Q-SDP evaluation kit for development purpose. I am unable to get Linux BSP package through LTIB. I follows i.MX_6Dual6Quad_Sabre-AI_Linux_User's_Guide.pdf, but when run the command ./ltib -m config get error zlib not installed.
However, I installed zlib "dpkg --get-selections | grep zlib*" returns
clisp-module-zlib install
gambas2-gb-compress-bzlib2 install
gambas2-gb-compress-zlib install
gauche-zlib install
libcompress-raw-zlib-perl install
libjzlib-java install
zlib-bin install
zlib-gst install
zlib1g install
zlib1g-dbg install
zlib1g-dev install
zlibc install
And this is the log of ./ltib -m config
Veriton-Series:~/freescale/source/ltib$ ./ltib -m config
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
zlib 0 not installed
Died at ./ltib line 1409.
traceback:
main::host_checks:1409
main:554
Exiting on error or interrupt
My host machine is ubuntu12.04, followed Setting_Up_LTIB_host.pdf instruction for setting of host machine but not getting.
Please help me to solve this issue.
Thanks,
Vidya
已解决! 转到解答。
Please, disable SSL by adding “--without-ssl” to the configure line in the *.spec file.
So:
1- In the file /ltib/dist/lfs-5.1/wget/wget.spec, at line “./configure”, add “--without-ssl”
2- once again, remove /opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1
3- run again ./ltib
Hi Yuri,
Since i have L3.0.35_4.1.0_130816_source file so copied required files in /opt/freescale/pkgs/
All files are:
1). m4-1.4.16.tar.gz
m4-1.4.16.tar.gz.md5
2).bison-2.6.tar.gz.md5
bison-2.6.tar.gz
flex, autoconfig, autolib, automake, lkc .
And finally got error, log is below:
Processing: distcc
====================i
Processing: ccache
====================
Processing: m4
================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: automake
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: wget
==================
Build path taken because: directory build, no prebuilt rpm,
Cowardly refusing to clobber existing directory:
/opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1
Remove this by hand if you really want to rebuild this package from scratch
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
What is the issue now could you suggest me to solve this issue.
Thanks,
Vidya
Hi Fernandez,
I installed today morning itself onpenssl, followed by same link, so openssl is not problem now.
I use ubuntu12.04 host machine i configured each and every thing as mentioned in pdf given by free scale, now where is the issue i am not able to find out, please help me.
Thanks,
Vidya
Please, disable SSL by adding “--without-ssl” to the configure line in the *.spec file.
So:
1- In the file /ltib/dist/lfs-5.1/wget/wget.spec, at line “./configure”, add “--without-ssl”
2- once again, remove /opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1
3- run again ./ltib
Hi Fernandez,
Thanks for helpful reply.
Today, i got menuconfig menu, changed for i.MX6 board.
but when i ran ./ltib command then got error regarding busybox
collect2: ld returned 1 exit status
make: *** [busybox_unstripped] Error 1
error: Bad exit status from /home/eldaas-dev/freescale/source/ltib/tmp/rpm-tmp.75361 (%build)
RPM build errors:
Bad exit status from /home/eldaas-dev/freescale/source/ltib/tmp/rpm-tmp.75361 (%build)
Build time for busybox: 4 seconds
Failed building busybox
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Thu Apr 24 18:11:40 2014
Ended: Thu Apr 24 18:11:45 2014
Elapsed: 5 seconds
These packages failed to build:
busybox
Build Failed
Please help to solve this issue.
Thanks,
vidya
Hi Fernandez,
Now i am trying to boot Linux BSP by use of SD card, follows "i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" and copied loader, uImage and rootfs in SD through MFG tools,
on u-boot console set environment
setenv loadaddr 0x10800000
setenv bootargs_lcd video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
setenv bootargs_base 'setenv bootargs console=ttymxc0,115200
setenv bootargs_mmc setenv bootargs ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
setenv bootcmd_mmc run bootargs_base bootargs_mmc;
mmc dev 2;
mmc read 0x10800000 0x800 0x2000;
setenv bootcmd run bootcmd_mmc
saveenv
run bootcmd
bootm
then kernel is loading but after sometime stopping
This is my pri command output on board :
MX6Q SABRESD U-Boot > pri
bootdelay=3
baudrate=115200
ipaddr=192.168.1.103
serverip=192.168.1.101
netmask=255.255.255.0
rd_loadaddr=(0x1300000)
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
nfsroot=/opt/eldk/arm
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
ethact=FEC0
bootargs=root=/dev/mmcblk0p1 rootwait rw
loadaddr=0x10800000
bootargs_lcd=video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_mmc=setenv bootargs ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
bootcmd_mmc=run bootargs_base bootargs_mmc
bootcmd=run bootcmd_mmc
stdin=serial
stdout=serial
stderr=serial
Environment size: 744/8188 bytes
MX6Q SABRESD U-Boot >
but kernel stops booting
log is below:
MX6Q SABRESD U-Boot > bootm
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-2666-gbdde708
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3866444 Bytes = 3.7 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 3.0.35-2666-gbdde708 (r65388@shlinux3) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PR3
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Ignoring unrecognised tag 0x54410008
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 194560
Kernel command line: ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 512MB 256MB = 768MB total
Memory: 765764k/765764k available, 282812k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xf4600000 - 0xffe00000 ( 184 MB)
vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x8003c000 ( 208 kB)
.text : 0x8003c000 - 0x80a8f8f4 (10575 kB)
.data : 0x80a90000 - 0x80af3e40 ( 400 kB)
.bss : 0x80af3e64 - 0x80b41d8c ( 312 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
console [tty0] enabled, bootconsole disabled
Please help me to solve this issue.
Thanks,
Vidya
Hi Vidya,
I think you haven't set up properly your U-Boot environment - your kernel command line is just:
Kernel command line: ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
For instance, in your setup this line is wrong:
setenv bootargs_mmc setenv bootargs ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
It should be something like:
setenv bootargs_mmc 'setenv bootargs ${bootargs} ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw'
In this way, when U-Boot runs bootcmd:
bootcmd_mmc=run bootargs_base bootargs_mmc
bootcmd=run bootcmd_mmc
the value of bootargs will be (bootargs_base + bootargs_mmc):
console=ttymxc0,115200 ip=192.168.1.104 root=/dev/mmcblk0p1 rootwait rw
I think you will have a similar issue regarding bootargs_lcd (although you are not using it).
Please, check carefully the documentation and your U-Boot environment, specially for 'typos'
Regards,
Gonzalo
Hi Gonzalo,
Thanks for reply,
I set environment on u-boot console as like
> setenv bootargs ' console=ttymxc0,115200 ip=dhcp root=/dev/mmcblk1p1 rootwait'
> setenv bootcmd 'mmc dev 2; mmc read ${loadaddr} 0x800 0x2100; bootm'
> saveenv
> boot
Kernel up but on LCD Linux icons do not come only four penguins come i tried to set
HannStar LVDS
on U-boot console by using the environment
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666'
but did not get LCD.
Second, in boot log shows
Mounting filesystems
cp: write error: No space left on device
why this error shows do not understand.
I attached log file please check ones.
Please suggest me how to solve this issue.
Thanks,
Vidya
Hi Vidya,
you say you have setup U-Boot environment for HannStar LVDS
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666'
and I thinks this should be OK for LVDS0 connection, but your log shows:
Kernel command line: console=ttymxc0,115200 ip=dhcp root=/dev/mmcblk1p1 rootwait
and that's not ok. Please, check again your U-Boot settings.
What rootfs are you trying to run?
Regarding "cp: write error: No space left on device", that's comming from user space. I think it probably comes from /etc/rc.d/init.d/filesystems, but I cannot help you on that; I don't have any board to try to see what's going on. You could try to add some "echo" statements to trace that message.
Regards,
Gonzalo.
P.S. Although the default is to mount the root device as read-write on boot, I would add rw to your kernel command line.
Hi Gonzalo,
I got LCD screen successfully, thanks for your suggestion.
As i am porting "L3.0.35_4.1.0_130816_source" and Linux "version 3.0.35-2666-gbdde708 " on i.MX6 processor, but not clear about which Linux flavour it is.
If i want to get Red Hat Linux flavour, what need to change in file system and kernel.
is any BSP is available with Linux Red Hat flavour, if available please suggest me.
Thanks,
Vidya
Hi Gonzalo,
I am compiling libmpeg2 but getting error, can you help me to solve this issue.
Log is below
Making all in libmpeg2
make[1]: Entering directory `/home/eldaas-dev/freescale/source/ltib/rpm/BUILD/mpeg2dec-0.4.1/libmpeg2'
Making all in convert
make[2]: Entering directory `/home/eldaas-dev/freescale/source/ltib/rpm/BUILD/mpeg2dec-0.4.1/libmpeg2/convert'
/bin/sh ../../libtool --tag=CC --mode=link gcc -Wall -g -O3 -fomit-frame-pointer -fno-common -prefer-non-pic -o libmpeg2convert.la -rpath /usr/lib -no-undefined rgb.lo uyvy.lo libmpeg2convertarch.la
gcc -shared .libs/rgb.o .libs/uyvy.o -Wl,--whole-archive ./.libs/libmpeg2convertarch.a -Wl,--no-whole-archive -Wl,-soname -Wl,libmpeg2convert.so.0 -o .libs/libmpeg2convert.so.0.0.0
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: .libs/rgb.o: relocation R_ARM_MOVW_ABS_NC against `a local symbol' can not be used when making a shared object; recompile with -fPIC
.libs/rgb.o: could not read symbols: Bad value
collect2: ld returned 1 exit status
make[2]: *** [libmpeg2convert.la] Error 1
make[2]: Leaving directory `/home/eldaas-dev/freescale/source/ltib/rpm/BUILD/mpeg2dec-0.4.1/libmpeg2/convert'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/eldaas-dev/freescale/source/ltib/rpm/BUILD/mpeg2dec-0.4.1/libmpeg2'
make: *** [all-recursive] Error 1
error: Bad exit status from /home/eldaas-dev/freescale/source/ltib/tmp/rpm-tmp.20628 (%build)
RPM build errors:
Bad exit status from /home/eldaas-dev/freescale/source/ltib/tmp/rpm-tmp.20628 (%build)
Build time for libmpeg2: 9 seconds
Failed building libmpeg2
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Thu May 15 17:56:44 2014
Ended: Thu May 15 17:57:21 2014
Elapsed: 37 seconds
These packages failed to build:
libmpeg2
Build Failed
Exiting on error or interrupt
Thanks,
Vidya
1) install patch-ltib-ubuntu12.04.sh from (https://community.freescale.com/docs/DOC-93455).
2) create a soft link under /usr/include.
sudo ln -s i386-linux-gun/sys sys
3) install additional packages.
sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev
sudo apt-get install texinfo
4) modify ltib/dist/lfs-5.1/base_libs/base_libs.spec.
...
perl -w -e '
# @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
# exit (0) unless @ARGV;
Hi Jiang,
Thanks for reply.
I did same as you said
1) ./L3.0.35_4.1.0_130816_source/install
got ltib directory then
2) cd ltib
installed install patch-ltib-ubuntu12.04.sh from (https://community.freescale.com/docs/DOC-93455).
./patch-ltib-ubuntu12.04.sh
--2014-04-15 19:00:36-- https://community.freescale.com/servlet/JiveServlet/downloadBody/93454-102-3-2834/ubuntu-ltib-patch....
Resolving community.freescale.com (community.freescale.com)... 204.93.78.236
Connecting to community.freescale.com (community.freescale.com)|204.93.78.236|:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 3364 (3.3K) [application/gzip]
Saving to: `ubuntu-ltib-patch.tgz'
100%[===============================================================================================================================>] 3,364 10.6K/s in 0.3s
2014-04-15 19:00:38 (10.6 KB/s) - `ubuntu-ltib-patch.tgz' saved [3364/3364]
ubuntu-ltib-patch/
ubuntu-ltib-patch/zlib.patch
ubuntu-ltib-patch/sparse-0.4-fixlabel.patch
ubuntu-ltib-patch/lkc-1.4-lib.patch
ubuntu-ltib-patch/mux_server.spec
ubuntu-ltib-patch/sparse-0.4-fixlabel.patch.md5
ubuntu-ltib-patch/install-patches.sh
ubuntu-ltib-patch/lkc.spec
ubuntu-ltib-patch/sparse.spec
ubuntu-ltib-patch/lkc-1.4-lib.patch.md5
cp lkc-1.4-lib.patch /opt/freescale/pkgs
cp lkc-1.4-lib.patch.md5 /opt/freescale/pkgs
cp sparse-0.4-fixlabel.patch /opt/freescale/pkgs
cp sparse-0.4-fixlabel.patch.md5 /opt/freescale/pkgs
Patching Spec Files
Done
patching file bin/Ltibutils.pm
eldaas-dev@eldaasdev-Veriton-Series:~/freescale/source/ltib$
3) cd /usr/include/
sudo ln -s i386-linux-gun/sys sys
4) installed
additional packages.
sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev
sudo apt-get install texinfo
5)
modified ltib/dist/lfs-5.1/base_libs/base_libs.spec.
...
perl -w -e '
# @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
# exit (0) unless @ARGV;
and
6). ./ltib -m config
eldaas-dev@eldaasdev-Veriton-Series:~/freescale/source/ltib$ ./ltib -m config
Installing host support packages.
This only needs to be done once per host, but may take up to
an hour to complete ...
If an error occurs, a log file with the full output may be found in:
/home/eldaas-dev/freescale/source/ltib/host_config.log
Exiting on error or interrupt
Please see >> /home/eldaas-dev/freescale/source/ltib/host_config.log for details
Please find error log below from (log_config.log).
Build time for rpm-fs: 130 seconds
sudo rpm --force-debian --root / --dbpath /tmp/rpm-eldaas-dev/rpmdb -e --allmatches --nodeps --define '_tmppath /home/eldaas-dev/freescale/source/ltib/tmp' rpm-fs 2>/dev/null
sudo rpm --force-debian --root / --dbpath /tmp/rpm-eldaas-dev/rpmdb --ignorearch -ivh --force --nodeps --excludedocs --define '_tmppath /home/eldaas-dev/freescale/source/ltib/tmp' /tmp/rpm-eldaas-dev/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm
Preparing... ##################################################
rpm-fs ##################################################
sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -Uv --justdb --notriggers --noscripts --nodeps /tmp/rpm-eldaas-dev/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm
error: failed to stat /home/eldaas-dev/.gvfs: Permission denied
Preparing packages for installation...
Processing platform: Host support packages
============================================
using /home/eldaas-dev/freescale/source/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Build path taken because: no prebuilt rpm,
Please reply asap why i am getting this error.
Thanks,
Vidya