MX6 Solo X Progressive display out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX6 Solo X Progressive display out

885件の閲覧回数
moowonlee
Contributor II

hi 

Does MX6SX support progressive display? 

MX6SX-----(Progressive, 8bits line)------>ADV7391 ------>RGB

is it possible?

ADV7391 supported Digital TV protocol standard.(SMPTE 293M, BTA T-1004, BT.1358, BT.1362)

0 件の賞賛
3 返答(返信)

702件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi moowon

yes it supports  YCbCr 4:2:2 format and this is described in

sect.37.4.11 ITU-R BT.656 Digital Video Interface (DVI) i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

702件の閲覧回数
moowonlee
Contributor II

i have a question

For progressive display out, would i add  Progressive modedb?

currently, i show modedb used.

static struct fb_videomode adv739x_modedb[] = {
{
/* NTSC Interlaced output */
"BT656-NTSC", 60, 720, 480, 37037,
.left_margin = 19, .right_margin = 3, /* interpreted as field 0 vertical top/bottom */
.upper_margin = 20, .lower_margin = 3, /* interpreted as field 1 vertical top/bottom */
.hsync_len = 276, .vsync_len = 1, /* htotal clocks = hsync_len + xres*2 */
.sync = FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
.vmode = FB_VMODE_INTERLACED,
.flag = FB_MODE_IS_DETAILED,},
{
/* PAL Interlaced output */
"BT656-PAL", 50, 720, 576, 37037,
.left_margin = 22, .right_margin = 2, /* interpreted as field 0 vertical top/bottom */
.upper_margin = 23, .lower_margin = 2, /* interpreted as field 1 vertical top/bottom */
.hsync_len = 288, .vsync_len = 1, /* htotal clocks = hsync_len + xres*2 */
.sync = FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
.vmode = FB_VMODE_INTERLACED,
.flag = FB_MODE_IS_DETAILED,},
};

0 件の賞賛

702件の閲覧回数
moowonlee
Contributor II

Hi igorpadykov

   

Thank you for response

I will try it !! 

0 件の賞賛