MX233 LCD flicker

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MX233 LCD flicker

575 次查看
yfwong1z
Contributor I

I have attached a 240x320 RGB LCD to MX233. LCDIF is configured to DOTCLK mode, pixel clock is 10Mhz and vsync is 60Hz.

The framebuffer driver is using double frame buffer. It is OK to display a still picture. As a test, the two buffers are initialized in different color. Then, I run a test app which calls ioctl FBIOPAN_DISPLAY to switch between the two buffers and flicker happens.

I have traced the driver, ioctl FBIOPEN_DISAPLY simply updates the register HW_LCDIF_NEXT_BUF. I am not sure if the flicker caused by updating HW_LCDIF_NEXT_BUF or some other reasons.

标记 (1)
0 项奖励
回复
0 回复数