Hi,
Does anyone has any idea of ODBS for EVK. This is On board diagnostic test for devices on EVK including DDR2, and all other chipsets. Please let me know if someone has already working on it. I have some issues with our custom board. I tried using OBDS for EVK on our board. It worked but it couldn't detect SPI NOT flash, PMIC, RTC, etc. But I could see DDR2 memmory test passed. This could be because of this ODBS is meant for EVK only. We may have to modify ODBS code for our custom i.MX51 board.
As far as I know, OBDS is only for FSL internal use and there is no support on it.