MT9D115 2M 照片分布错乱 (复现概率:50%)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MT9D115 2M 照片分布错乱 (复现概率:50%)

5,585 Views
xingruizhu
Contributor III

Dear supporter

在我们的案子(android4.2.2 upgrade to android 5.0.2)上使用2M camera (Sensor MT9D115)拍照,获得的照片有时会很奇怪:有些画面产生了错乱(请参见附件),复现概率大概有50%

请问有哪些测试分析点可以定位问题的来源?

另外sensor本身应该无问题,因为同一台机器,刷android 4.2的镜像就没有问题,刷android 5.0.2就出现上述问题.

问题很紧急,请帮忙分析一下,给一些debug的方向.

感谢.

- Camera Sensor相关规格 -

Focusing Type: Fix Focusing
Frame Rate: SXGA@15fps
System Interface: Parallel

- 项目平台信息 -

  • IMX6DL
  • Android 5.0.2

0 Kudos
4 Replies

5,271 Views
liyu1
Contributor III

请问您这个问题解决了吗?,我也是用的美光的sensor mt9d112 也是跟你同样的问题

0 Kudos

5,271 Views
liyu1
Contributor III
0 Kudos

5,271 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Xingrui,

    I can only give you some limited advice, because the camera you are using is not supported by EVK board, I don't have environment to test it.

attachments are 2 patches, you can try to patch them to your system. Remind you had better backup corresponding files before patching.

Regards,

weidong

0 Kudos

5,271 Views
xingruizhu
Contributor III

Dear supporter

With some hardwork, the below config should be set in function vidioc_int_g_ifparm_num()

p->u.bt656.nobt_vs_inv = 1;

could give us more explanation about the rootcause ?

0 Kudos