MPU Reset/Power under PMU control or external PMIC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPU Reset/Power under PMU control or external PMIC

ソリューションへジャンプ
689件の閲覧回数
kaveeh
Contributor I

Hi,

there are two methods to connect the Push button for power-up sequence and top-level reset. One, by connecting the push button to the ONOFF pin of the IMX and then PMIC will power-up with the PMIc_on_REG. Other is by connecting the Push button directly to the PMIC.

Is there any significant advantage/disadvantage between these two methods?

Thanks

pastedImage_0.png

pastedImage_1.png

ラベル(2)
0 件の賞賛
返信
1 解決策
552件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

It really it is just an option to the implementation, but  there is no a real advantage or disadvantage one I can said  adding the push-button into the i.MX instead of the PMIC it is to implement a 3 seconds suspend, like in the laptops power button. But it is basically the same approach.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
553件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Kaveh,

It really it is just an option to the implementation, but  there is no a real advantage or disadvantage one I can said  adding the push-button into the i.MX instead of the PMIC it is to implement a 3 seconds suspend, like in the laptops power button. But it is basically the same approach.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信