MMPF0100 how to enter OFF mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 how to enter OFF mode

1,403件の閲覧回数
peterhygren
Contributor III

We've developed a custom board with IMX6D and MMPF0100 (default version) and are running a yocto custom build. We have a problem with power off mode, we can't enter it. We're not interested in sleep or standby etc.

The datasheet for MMPF0100 states that if PWRON is set low and SWxOMODE bits are not set, OFF mode should be entered, however the voltages (SW1-4 and VGEN1-6) won't shut off so I assume sleep is entered. However I am seeing some weird behavior in SW2, namely it alternates between 1.8V and 2.2V.

The power button is connected to the CPU and I see no difference between "shutdown -h 0" and just asserting the power button for >4s.

Any ideas?

ラベル(4)
0 件の賞賛
返信
0 返答(返信)