MMPF0100: Discrepancy between Dual-lite Sabre and AN4536

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMPF0100: Discrepancy between Dual-lite Sabre and AN4536

672 次查看
Sebster
Contributor II

Hello Community,

Per AN4536 and datasheet, the F0 variant column identifies a selected voltage of 3.3V on SW2 whereas the SABRE ref design identifies the voltage as 3.0V.   Can you confirm is this MMPF0100 variant default is 3.0V, or has the PMIC used in SABRE Dual-Lite been altered from the F0 pre-programming?

Same oberversation for SABRE Dual-Lite the SW4 output at 1.8V, whereas the datasheet table indicates a voltage of 3.15V for F0. Again this must have been altered right?

Thanks

Seb

标签 (2)
0 项奖励
回复
1 回复

553 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sebastien

yes, SW voltages can be changed at run time.

MMPF0100 F0 (preprogrammed)  has SW2 3.3V, SW4 3.15 

Table 10. Start-up Configuration MMPF0100

below part of Sabre SDP, MCIMX6DL-SDP,   SPF-27392  p.19

i.MX6_SABRE_SDP_DESIGNFILES

SPF-27392  p.19.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复