MMC standby issue for WiFI on imx6dl board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMC standby issue for WiFI on imx6dl board

1,813 Views
mrleo
Contributor IV

Hi,all

I debug rtl8723 sdio module in android 4.4.2 system on on imx6dl board,I found that if system enter standby,after a while,resume the system.

It can not enable the wifi.

I think this is mmc standby issue about sd_write32 error.

What should I do to solve this problem?

Below are  error messages:

RTL871X: module init start

RTL871X: rtl8723bs v4.3.5_11545.20140603_BTCOEX20140507-4E40

RTL871X: build time: Nov 10 2014 17:41:13

RTL871X: rtl8723bs BT-Coex version = BTCOEX20140507-4E40

RTL871X: register rtw_netdev_ops to netdev_ops

RTL871X: rtw_wdev_alloc(padapter=dfdf1000)

RTL871X: Chip Version Info: CHIP_8723B_Normal_Chip_TSMC_B_CUT_1T1R_RomVer(0)

RTL871X: RF_Type is 3!!

RTL871X: EEPROM type is E-FUSE

RTL871X: SetHwReg8723B: bMacPwrCtrlOn=1

RTL871X: _ReadAdapterInfo8723BS, 0x4e=0xe0

RTL871X: hal_EfuseSwitchToBank: Efuse switch bank to 0

RTL871X: hal_ReadEFuse_WiFi: data end at address=0xab

RTL871X: Efuse Realmap:

29 81 03 7C 51 08 28 00 62 07 0D 45 10 00 00 00

31 31 32 32 32 32 33 33 34 34 34 EE FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF 2D 2D 2D 2D 2D 2D

2D 2D 2D 2D 2D E0 FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF 20 2D 1E 00 33 88 FF FF

FF 29 20 11 00 00 00 FF 00 FF 12 FF FF FF FF FF

3E 10 01 02 23 00 00 FF 20 04 4C 02 23 B7 21 02

0C 00 22 04 00 08 00 32 FF 21 02 0C 00 22 2A 01

01 00 00 00 00 00 00 00 00 00 00 00 02 00 FF FF

00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

00 EB 00 6E 01 00 00 00 00 FF 08 D8 33 D9 E9 6D

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

RTL871X: Hal_EfuseParseBTCoexistInfo_8723B: Enable BT-coex, ant_num=1

RTL871X: Hal_EfuseParsePackageType_8723B phy efuse read 0x1FB =fc

RTL871X: PackageType = 0x4

RTL871X: Hal_EfuseParseVoltage_8723B hwinfo[EEPROM_Voltage_ADDR_8723B] =62

RTL871X: Hal_EfuseParseVoltage_8723B pEEPROM->adjuseVoltageVal =6

RTL871X: AutoloadFail =0,

RTL871X: Adapter->eeprompriv.EEPROMRFGainVal=f0

RTL871X: EEPRORFGainOffset = 0x29

RTL871X: SetHwReg8723B: bMacPwrCtrlOn=0

RTL871X: <==== _ReadAdapterInfo8723BS in 790 ms

RTL871X: init_channel_set ChannelPlan ID 20 Chan num:13

RTL871X: rtw_register_early_suspend

RTL871X: Init_ODM_ComInfo_8723b(): fab_ver=0 cut_ver=0

RTL871X: rtw_macaddr_cfg MAC Address  = 08:d8:33:d9:e9:6d

RTL871X: bDriverStopped:1, bSurpriseRemoved:0, bup:0, hw_init_completed:0

RTL871X: register rtw_netdev_ops to netdev_ops

RTL871X: register rtw_netdev_if2_ops to netdev_ops

RTL871X: rtw_wdev_alloc(padapter=dfe5f000)

RTL871X: Chip Version Info: CHIP_8723B_Normal_Chip_TSMC_B_CUT_1T1R_RomVer(0)

RTL871X: RF_Type is 3!!

RTL871X: init_channel_set ChannelPlan ID 20 Chan num:13

RTL871X: rtw_ndev_init(wlan0)

RTL871X: _rtw_drv_register_netdev, MAC Address (if1) = 08:d8:33:d9:e9:6d

RTL871X: rtw_ndev_init(p2p0)

RTL871X: _rtw_drv_register_netdev, MAC Address (if2) = 0a:d8:33:d9:e9:6d

RTL871X: module init ret=0

RTL871X: +871x_drv - if2_open, bup=0

RTL871X: +871x_drv - drv_open, bup=0

RTL871X: SetHwReg8723B: bMacPwrCtrlOn=1

RTL871X: <3>sd_write32: (-84) addr=0x10948 val=0x00000280

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=0

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=1

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=2

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=3

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=4

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=5

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=6

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=7

RTL871X: <3>sd_write32: FAIL!(-84) addr=0x10948 val=0x00000280, try_cnt=8

RTL871X: rtl8723b_FirmwareDownload fw: FW_NIC, size: 30808

RTL871X: rtl8723b_FirmwareDownload: fw_ver=1b fw_subver=0001 sig=0x5301, Month=04, Date=29, Hour=13, Minute=45

RTL871X: rtl8723b_FirmwareDownload(): Shift for fw header!

RTL871X: <3>sd_write32: (-84) addr=0x11000 val=0x02ed4502

RTL871X: <3>sd_write32: (-84) addr=0x11000, val=0x2ed4502, try_cnt=0

RTL871X: [dvobj:d7137000][ERROR] continual_io_error:9 > 8

RTL871X: <3>sd_write32: (-84) addr=0x11000 val=0x02ed4502, try_cnt=0

====>_BlockWrite 110 i:0

====>_WriteFW 248

RTL871X: FWDL fail. write_fw:1, 0ms

RTL871X:  <=== rtl8723b_FirmwareDownload()

RTL871X: rtw_hal_init: hal__init fail

RTL871X: -871x_drv - drv_open fail, bup=0

RTL871X: -871x_drv - if2_open, bup=0

ADDRCONF(NETDEV_UP): p2p0: link is not ready

RTL871X: cfg80211_rtw_set_power_mgmt(p2p0) enabled:1, timeout:-1

RTL871X: cfg80211_rtw_flush_pmksa(p2p0)

RTL871X: cfg80211_rtw_change_station(p2p0)

RTL871X: cfg80211_rtw_change_station(p2p0)

RTL871X: cfg80211_rtw_change_station(p2p0)

RTL871X: +871x_drv - drv_open, bup=0

RTL871X: <3>sd_write32: (-84) addr=0x10948 val=0x00000280

RTL871X: <3>sd_write32: (-84) addr=0x10948, val=0x280, try_cnt=0

RTL871X: [dvobj:d7137000][ERROR] continual_io_error:10 > 8

RTL871X: <3>sd_write32: (-84) addr=0x10948 val=0x00000280, try_cnt=0

RTL871X: rtl8723b_FirmwareDownload(wlan0) tmp_ps=0

RTL871X: rtl8723b_FirmwareDownload fw: FW_NIC, size: 30808

RTL871X: rtl8723b_FirmwareDownload: fw_ver=1b fw_subver=0001 sig=0x5301, Month=04, Date=29, Hour=13, Minute=45

RTL871X: rtl8723b_FirmwareDownload(): Shift for fw header!

RTL871X: _FWDownloadEnable: !!!!!!!!Write 0x80 Fail!: count = 101

RTL871X: _8051Reset8723: Finish

RTL871X: _FWFreeToGo: Polling FW ready Fail! (1, 0ms), REG_MCUFWDL:0x00000001

RTL871X: FWDL fail. write_fw:0, 10ms

RTL871X:  <=== rtl8723b_FirmwareDownload()

RTL871X: rtw_hal_init: hal__init fail

RTL871X: -871x_drv - drv_open fail, bup=0

RTL871X: cfg80211_rtw_change_station(p2p0)

RTL871X: cfg80211_rtw_change_station(p2p0)

RTL871X: LeaveAllPowerSaveMode(p2p0): bup=0 Skip!

RTL871X: rtw_p2p_enable: bDriverStopped=0, bup=0, hw_init_completed=0

Thanks,

Leo

Labels (4)
3 Replies

788 Views
ct3paul
Contributor II

Hi mrleo!

I also want to debug rtl8723 sdio module on I.MX6Q.

Are there some schematics and programs can give some helps?

Thank you very much!

Chen

0 Kudos
Reply

788 Views
mrleo
Contributor IV

Hi,all

Wifi rtl8723as no hardware cd detect,how to wake up sdio?

When I enabled  wifi,after suspend,resume the system,wifi driver can wake up sdio.

If not enabled wifi,after suspend,resume the system,enabled wifi,will be not ok.

I think it is not found sdio.

How to detect wifi sdio?

Thanks,

Leo

788 Views
mrleo
Contributor IV

Hi all,

I found that if not enable the wifi or connected the wifi,enter suspend,later resume the system. The sdio is not detected.

like belwo:

cat /sys/kernel/debug/mmc2/ios

clock:          400000 Hz

vdd:            21 (3.3 ~ 3.4 V)

bus mode:       1 (open drain)

chip select:    0 (don't care)

power mode:     2 (on)

bus width:      0 (1 bits)

timing spec:    0 (legacy)

Thanks,

Leo

0 Kudos
Reply