Hello,
I'm trying to use MINISASTOCSI MIPI camera with NXP IMX8M Quad EVK on Android.
The Android version is: 8.1.0 1.3.0-rfp-rc3 20180406.
The camera is no working and the camera app is closing directly after I confirm the location question in the app.
In the Quick Start Guide for MINISASTOCSI for i.MX 8M Evaluation Kit no futher information for Android are described.
Regards
Urs
Hi Urs
one can try Demo Image
just for checking hardware one can test it with linux using AN12187 Quick Start Guide for MINISASTOCSI for i.MX 8M Evaluation Kit
https://www.nxp.com/docs/en/application-note/AN12187.pdf
Best regards
igor
Hi Urs
I checked internally, there are no known issues with camera in linux/android.
One can try to test hardware using links
Yocto release for i.MX 8MQ - Boundary Devices
DART-MX8M CSI - Variscite Wiki
Best regards
igor
Hi Urs
there is limitation for camera described in Table 2. Features attached Release Notes p.3
"OV5640. Camera cannot co-work with MIPI Display due to the I2C address conflict."
Also one can consider fsl-imx8mq-evk-mipi-csi2.dtb in mfg tools:
Manufacturing Toolkit for Android O8.1.0_1.3.0 8MQ GA
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------