MINISASTOCSI MIPI camera not working with Android on i.MX8M Quad EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MINISASTOCSI MIPI camera not working with Android on i.MX8M Quad EVK

2,030 Views
geser_u
Contributor I

Hello,

 

I'm trying to use MINISASTOCSI MIPI camera with NXP IMX8M Quad EVK on Android.

The Android version is: 8.1.0 1.3.0-rfp-rc3 20180406.

The camera is no working and the camera app is closing directly after I confirm the location question in the app.

In the Quick Start Guide for MINISASTOCSI for i.MX 8M Evaluation Kit no futher information for Android are described.

  • Is for Android any configuration required?
  • How can I check that the camera is working?

Regards

Urs

Labels (1)
0 Kudos
5 Replies

1,610 Views
geser_u
Contributor I

Hi Igor,

We use a HDMI monitor. 

Why the camera doesn't work together with the HDMI monitor?

Best regards

Urs

0 Kudos

1,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Urs

one can try Demo Image

https://www.nxp.com/webapp/Download?colCode=O8.1.0_1.3.0_ANDROID_DEMO_8MQ_GA&appType=license&locatio... 

just for checking hardware one can test it with linux using AN12187 Quick Start Guide for MINISASTOCSI for i.MX 8M Evaluation Kit
https://www.nxp.com/docs/en/application-note/AN12187.pdf

Best regards
igor

0 Kudos

1,610 Views
geser_u
Contributor I

Hi Igor,

I have download the Demo Images – i.MX 8MQuad EVK again with the MGFTool. The download was successful, but the camera don't work.

Best regards

Urs

0 Kudos

1,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Urs

I checked internally, there are no known issues with camera in linux/android.

One can try to test hardware using links

i.MX8M Camera commands 

Yocto release for i.MX 8MQ - Boundary Devices 

DART-MX8M CSI - Variscite Wiki 

Best regards
igor

0 Kudos

1,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Urs

there is limitation for camera described in Table 2. Features attached Release Notes p.3

"OV5640. Camera cannot co-work with MIPI Display due to the I2C address conflict."

Also one can consider fsl-imx8mq-evk-mipi-csi2.dtb in mfg tools:

Manufacturing Toolkit for Android O8.1.0_1.3.0 8MQ GA

https://www.nxp.com/webapp/Download?colCode=O8.1.0_1.3.0_ANDROID_TOOL_8MQ_GA&appType=license&locatio... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos