MIMXRT1040-EVK LCDIF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1040-EVK LCDIF

496 次查看
tbonkers
Contributor II

I am trying to connect an LCD RK043FN66HS-CTG to MIMXRT1040-EVK, using Zephyr and LVGL. Managed to compile the source using the MIMXRT1050-EVK port as a guide however the TFT does not show anything at all.

The schematic of the evaluation kit shows the LCD data lines multiplexed with other signals. Should I remove them 0-ohm resistors from these lines, so the LCDIF peripheral has full control over them?

0 项奖励
回复
2 回复数

478 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

476 次查看
tbonkers
Contributor II
I did use the 1050 code as a guide. The LVGL demo app boots up and the display lights up. The console shows "- display-controller@402b8000 (READY)
", however the display is all white.

The zephyr.dts file contains the following:

pinmux_lcdif: pinmux_lcdif {
phandle = < 0x10d >;
group0 {
pinmux = < &iomuxc_gpio_b0_00_lcdif_clk >, < &iomuxc_gpio_b0_01_lcdif_enable >, < &iomuxc_gpio_b0_02_lcdif_hsync >, < &iomuxc_gpio_b0_03_lcdif_vsync >, < &iomuxc_gpio_b0_04_lcdif_data00 >, < &iomuxc_gpio_b0_05_lcdif_data01 >, < &iomuxc_gpio_b0_06_lcdif_data02 >, < &iomuxc_gpio_b0_07_lcdif_data03 >, < &iomuxc_gpio_b0_08_lcdif_data04 >, < &iomuxc_gpio_b0_09_lcdif_data05 >, < &iomuxc_gpio_b0_10_lcdif_data06 >, < &iomuxc_gpio_b0_11_lcdif_data07 >, < &iomuxc_gpio_b0_12_lcdif_data08 >, < &iomuxc_gpio_b0_13_lcdif_data09 >, < &iomuxc_gpio_b0_14_lcdif_data10 >, < &iomuxc_gpio_b0_15_lcdif_data11 >, < &iomuxc_gpio_b1_00_lcdif_data12 >, < &iomuxc_gpio_b1_01_lcdif_data13 >, < &iomuxc_gpio_b1_02_lcdif_data14 >, < &iomuxc_gpio_b1_03_lcdif_data15 >;
drive-strength = "r0-6";
input-schmitt-enable;
bias-pull-up;
bias-pull-up-value = "100k";
slew-rate = "slow";
nxp,speed = "100-mhz";
};
group1 {
pinmux = < &iomuxc_gpio_ad_b1_03_gpio1_io19 >, < &iomuxc_gpio_b1_15_gpio2_io31 >;
drive-strength = "r0-6";
slew-rate = "slow";
nxp,speed = "100-mhz";
};
};
};

Is there something obviously wrong?
0 项奖励
回复