MCIMX6ULL_CM Q701 RYU002N05 Mosfet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6ULL_CM Q701 RYU002N05 Mosfet

990件の閲覧回数
maticmohorcic
Contributor II

I'm checking MCIMX6Y2DVM09AB reference design MCIMX6ULL (SCH-29364_A1) and I do not why why there are two different type of N mosfet used (Q701, Q702) for adding parallel resistors (R707, R708). There are Q701 RYU002N05 and Q702 2SK3018.  PMIC_STBY_REQ drives Q701 drives and GPIO_DVFS drives Q702.

0 件の賞賛
5 返答(返信)

985件の閲覧回数
Yuri
NXP Employee
NXP Employee

@maticmohorcic 
Hello,

   i.MX 6ULL Linux supports such features as CPU Frequency Scaling (CPUFREQ),
Dynamic Bus Frequency. Also low power modes can be used. All these features
allow to decrease CPU voltage. 

Regards,
Yuri.

980件の閲覧回数
maticmohorcic
Contributor II

@Yuri

I undestand that but why different type N mosfet (Q701 RYU002N05 and Q702 2SK3018) are used (in parallel feedback resistor circuit) ?

 

0 件の賞賛

935件の閲覧回数
Yuri
NXP Employee
NXP Employee

@maticmohorcic 
Hello,

     Q702 (2SK3018) has leakage of 1uA (R708 of 1.5M).

https://pdf1.alldatasheet.com/datasheet-pdf/view/173401/ROHM/2SK3018.html

    Q701 (RYU002N05) - leakage of 10 uA (R707, 147K)

https://pdf1.alldatasheet.com/datasheet-pdf/view/429927/ROHM/RYU002N05.html


 Regards,
Yuri

929件の閲覧回数
maticmohorcic
Contributor II

@Yuri 

Why RYU002N05 is equipped on PMIC_STBY_REQ and it has higher gate-source leakage current (10uA - 2SK3018 has 1uA), so turned on when standy request is enabled.

0 件の賞賛

912件の閲覧回数
Yuri
NXP Employee
NXP Employee

@maticmohorcic 
Hello,

  threee working points are available for VDD_ARM_SOC_IN: 1.4V, 1.3V, 0.925V
Look at the comments on the scheme (regarding R1/R2). To get 0.925V - 1.5 Mohm 
is needed as a shunt; for 1.3V - 147 Kohm is enough. 

Regards,
Yuri.

0 件の賞賛