MCIMX6SLEVK, what is the function of the AC14 pin (REF_CLK_24M) connection between the processor and the PF0100 (INTB)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6SLEVK, what is the function of the AC14 pin (REF_CLK_24M) connection between the processor and the PF0100 (INTB)?

ソリューションへジャンプ
882件の閲覧回数
RobertCorrellus
Contributor II

MCIMX6SLEVK,  what is the function of the AC14 pin (REF_CLK_24M) connection between the processor and the PF0100 (INTB)?

ラベル(1)
タグ(3)
1 解決策
737件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Pin INTB is the open drain interrupt signal from PF0100 to processor. On EVK, this pin is connecting to REF_CLK_24M which is selected as GPIO input GPIO3_IO21 by default.

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
738件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Pin INTB is the open drain interrupt signal from PF0100 to processor. On EVK, this pin is connecting to REF_CLK_24M which is selected as GPIO input GPIO3_IO21 by default.

0 件の賞賛
737件の閲覧回数
RobertCorrellus
Contributor II

Thanks for your quick reply.  The interrupt from the PF0100 is open drain to the processor, should there be a pull-up on the line?

0 件の賞賛
737件の閲覧回数
PeterChan
NXP Employee
NXP Employee

It is optional to have external pull-up on the line because the pad REF_CLK_24M has internal pull-up which can be configured in the IOMUXC_SW_PAD_CTL_PAD_REF_CLK_24M register.

0 件の賞賛