MCIMX6Q-SDP fals boot rarely.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6Q-SDP fals boot rarely.

912件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have some question about i.MX6 SABRE platform.

Rarely, MCIMX6Q-SDP cannot boot correctly with a error (virtual address error) similar to the attached file.

=====

[Board]

MCIMX6Q-SDP

[BSP]

jb4.2.2_1.0.0-ga

[Procedure]

1. Boot Android 4.2 BSP.

2. After boot, execute a command "reboot -p" to power off.

3. After power off, push power button to reboot.

4. Repeat 2, 3 procedure.

=====

[Q]

Do you have a solution to resolve this issue?

Best Regards,

Satoshi Shimoda

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

813件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Which error have you met when you boot ? And about the android image you built yourself or demo image from freescale?

Have a nice day~~

Best Regards

Dan

0 件の賞賛
返信

813件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Dan,

Sorry, I forgot attaching file.

This issue was occurred with freescale pre-built image.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信

813件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

The demo image is default boot from eMMC. If you want to boot from SD card, you need to modify somethings. If using the default image without any changes , errors come. So here I recommend you to burn the images to eMMC and boot from it.

You can have a try.

Best Regards

Dan

0 件の賞賛
返信

813件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Where have you burned the image to ? SD card or eMMC?

Best Regards

Dan

0 件の賞賛
返信