Hi community,
I have some question about i.MX6 SABRE platform.
Rarely, MCIMX6Q-SDP cannot boot correctly with a error (virtual address error) similar to the attached file.
=====
[Board]
MCIMX6Q-SDP
[BSP]
jb4.2.2_1.0.0-ga
[Procedure]
1. Boot Android 4.2 BSP.
2. After boot, execute a command "reboot -p" to power off.
3. After power off, push power button to reboot.
4. Repeat 2, 3 procedure.
=====
[Q]
Do you have a solution to resolve this issue?
Best Regards,
Satoshi Shimoda
Hi Satoshi,
Which error have you met when you boot ? And about the android image you built yourself or demo image from freescale?
Have a nice day~~
Best Regards
Dan
Hi Satoshi,
The demo image is default boot from eMMC. If you want to boot from SD card, you need to modify somethings. If using the default image without any changes , errors come. So here I recommend you to burn the images to eMMC and boot from it.
You can have a try.
Best Regards
Dan
Hi Satoshi,
Where have you burned the image to ? SD card or eMMC?
Best Regards
Dan