MCIMX6Q-SDB/nSRST of JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDB/nSRST of JTAG

554 Views
soichiyamamoto
Contributor V

Hi,

There is a question about JTAG circuit of MCIMX6Q-SDB.

Follows are nSRST specifications.

  nSRST(Input/output)

     Active Low output from RealView ICE to the target system reset, with a 4.7kΩ pull-up resistor for de-asserted state.

     This is also an input to RealView ICE so that a reset initiated on the target can be reported to the debugger.

     This pin must be pulled HIGH on the target to avoid unintentional resets when there is no connection.

However, in MCIMX6Q-SDB, it does not support the following specifications.

    ・This is also an input to RealView ICE so that a reset initiated on the target can be reported to the debugger.

無題.jpg

Q1)What is the reason?

Best Regards,

soichi

Labels (2)
0 Kudos
1 Reply

427 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

reason is that there is no reset button on board. Also according to arm faq

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/ka3895.html

"It is not strictly necessary to connect nSRST..".

If necessary one can add this using Figure 2-3 Example reset circuit logic

arm document DAI0072A_multiicedesign_notes.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos