MCIMX28EVKJ: i.MX28 Evaluation Kit SD card slots

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX28EVKJ: i.MX28 Evaluation Kit SD card slots

818件の閲覧回数
ganeshh
Contributor III

hello,

In i.MX28 Evaluation kit can i use bothe sd card slots at the same time that is one for loading os and other for connectiong some sdio device say a sdio Bluetooth device can i do both these functions at the some time. In i.MX28 Evealuations Harware Users guide i saw boot mode options are set using four switches.Its different number for accessing each sd card slot. Is possible to access both together

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

685件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The i.MX28 EVK is equipped with two independent SD ports :

SD0 and SD1 can both be used separately, say as boot devices.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

685件の閲覧回数
ganeshh
Contributor III

Hello Yuri Muhin,

Am asking that am booting from SD0 and can i use SD1 simultaneously as a Bluetooth/WIFI device. For an example something like this http://www.silexamerica.com/products/connectivity-solutions/embedded-wireless/radio-modules/sx-sdcan...

0 件の賞賛
返信

685件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes. It is possible to boot "from SD0 and use SD1 simultaneously as a Bluetooth/WIFI device"

685件の閲覧回数
ganeshh
Contributor III

Thanks Yuri,

But what will be the condition of boot switch at that time?

0 件の賞賛
返信