Hai all,
we designed a custom board same as iMX6SLEVK board .it has both sdcard and eMMC boot selection and flashed images of Android4.4.2 to eMMC & sdcard successfully.
Then we tried Yocto(3.10.17) core-minimal-images and successfully flashed to the sdcard but unable to flash to eMMC.
Now inorder to flash yocto images to eMMC what are the changes we have to do in the kernel and uboot level.
Thanks and Regards,
D.jansirani
Hi Jansi
one can use Mfg Tools for eMMC programming
i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0)
https://www.nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL&appType=license&location=n...
or erase partitions as suggested on
https://community.nxp.com/thread/435725
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the quick reply.
we are already using i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0) to flash yocto images to the sdcard without any problem.
As the yocto default source code for iMX6SL compiles images for sdcard .
now we want to know what are the changes we have to do in kernel and uboot source code inorder to compile images (rootfs+uImage+uboot) to flash to eMMC Flash?
Note :
just to update i.MX 6Family Manufacturing Toolkit for L3.10.17 (REV L3.10.17_1.0.0) downloaded one will have the Mfgfirmware images for sdcard so we have to compile the uboot and uImage for the Mfg firmware also inorder to flash to eMMC.