Hi,
I have a Segger J-Link and openocd and got a connection running with my imx28evk-board.
Now I want to load U-boot to memory with JTAG so I can run it directly and not have to read it from sdcard, however I haven't found any documentation on how to do this. I have moved the switches to JTAG boot mode and tried to follow something like this guy did https://community.nxp.com/message/307083
but the only output I got from my evk-board was this:
U-Boot 2013.07-rc2-00023-ga544ead (Jul 04 2013 - 15:30:51)
CPU: Freescale i.MX28 rev1.2 at 454 MHz
BOOT: Û_©ÌÚ^)×
´®»!2¡ vm^
Á
;b2&¿ù1LÉ~éJ
`m
ÆãäÉê$1³ÿbd軼vþ¾_^Òo?+k
ÃÊôã»ÆZPÜxÿ¥
¸'pfE¾¤à®zÇt¹5Ù,HíÈ&>©ãsë¢ö]®mïÃþòÏÛk=-_ÎÙ®|~ £Gô'?J;î-
R¯CabsRØäÿkèDk2:Gfø^ÂùµüÄù¾
ʶ"¼÷ñÛÕxÞfêÈ
As you may notice I have compiled mainline U-boot and it seems to start but then turns into random crap. Do you have any idea of what I'm doing wrong here?
已解决! 转到解答。
Hi rajtantajtan,
it is no problem to load U-Boot into RAM via JTAG. Just load and execute i.MX28's U-Boot SPL ELF before normal U-Boot ELF. After SPL was execiuted DDR is initialized and normal U-Boot ELF could be loaded to DDR.
SPL ELF could be found in subfolder SPL of U-Boot source tree.
Regards,
Christoph
Is this perhaps a baudrate issue ? You are using your terminal emulator with a baudrate, then u-boot starts and set it to another value and your terminal emulator stays with the older setting. Try changing the baudrate of your terminal emulator or find out what u-boot setting is. Just an idea ..