Linux freez when MIPI & M4 are used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux freez when MIPI & M4 are used

1,489 Views
urimashiach
Contributor III

Hello

Hardware: i.MX 7Dual revision 1.2 and 1.3

Software: Linux, based on NXP 4.14.98-2.0.0_ga.

Scenario:

* The M4 core is executing a program that continuously generates UART messages and changing the value of a GPIO.

* The MIPI display is active.

* The ambient temperature is 45 degrees Celsius.

* The measured temperature, by the A7, is 75C.

The following command is used to read the A7 temperature:

# cat /sys/class/thermal/thermal_zone0/temp

* The Linux get stuck after a few minutes.

* The problem doesn't occur if the M4 or the LVDS is not active.

* Some SOCs requires a higher temperature to recreate the problem.

Please let me know if additional information is needed.

Thanks,

Uri

Labels (3)
Tags (1)
4 Replies

1,345 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Uri,

Have you considered the procedure mentioned on section 2.8.5 of the i.MX Linux Reference Manual document (IMXLXRM Rev. L4.14.98-2.0.0_ga), and also, the notes of Table 10 regarding the proper DTB Description according with the board revision on i.MX Linux Release Notes document (IMXLXRN Rev. L4.14.98-2.0.0_ga)?

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

---------------------------------------------------------------------------

0 Kudos

1,345 Views
urimashiach
Contributor III

Hi Carlos,

The SOC operation frequency was limited to 996MHz.
We are unable to reproduce the problem with SOC frequency of 996MHz.

Thank you for your help.

0 Kudos

1,345 Views
urimashiach
Contributor III

Hi Carlos,

Thank you for your help.

Please provide links to the documents from your reply:

* MXLXRM Rev. L4.14.98-2.0.0_ga

* IMXLXRN Rev. L4.14.98-2.0.0_ga

Thanks,

Uri

0 Kudos

1,345 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Uri,

These documents are part of the Linux BSP documentation package, available on the following link:

https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga

 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

---------------------------------------------------------------------------

0 Kudos