So, I am trying to use this linphone 3.7.0 on my Sabre platform for smart devices with OV5640 mipi camera.
I have done these steps:
1. Compile Linux BSP 4.0.1 3.0.35 from freescale
2. Compile linphone, ortp, mediastreamer2 for imx6q
3. Launch linphone, using "linphonec -V -d 3"
The problem is that I can see nothing on a self view (only a black screen). It seems like issue in Xv library which I have taken from freescale Ubuntu image (Linux BSP has not this library)
This phrase I see in linphone debug:
"ortp-error-Could not find suitable format or Xv port to work with."
I have attached the linphone log.
So, from this point I need some help to understand a causes of this problem. And I will appreciate for any advices!
Thanks...
Original Attachment has been moved to: linphone_log.txt.zip
Hi,
I am facing the same issue with linphone 3.10.2 version on imx6. Were you able to find a solution for this problem ? It'd be of great help as I am stuck on this issue for a long time.
Thanks
Hi Konstantin, seems some libraries are missed,
suggest to use latest Freescale yocto
L3.10.17_1.0.0_IMX6QDLS_BUNDLE
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
So, now I have built the linphone with latest freescale yocto project (i.MX6Q: i.MX 6Quad Processors – Quad Core) and I have the same issue like in my first post. I mean this "ortp-error-Could not find suitable format or Xv port to work with."
Unfortunately, I was forced to downgrade the linphone from 3.7.0 to 3.6.1 version because of some obstacles during the compilation process which I couldn't overcome... (I can't build "antlr3-3.4" for belle-sip, for instance). It seems like problem between vivante video driver and Xv in Xserver. However, I don't know how to handle it and I need help! Perhaps, there are people here who worked with Xv and vivante, so please tell me, what should I do on a next step?
Here my xorg.conf:
*************************************************************
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "vivante"
Option "fbdev" "/dev/fb0"
Option "vivante_fbdev" "/dev/fb0"
Option "HWcursor" "false"
EndSection
Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection
*************************************************************
Here my xserver configuration flags:
*********************************************************************************************************************
EXTRA_OECONF += "--with-fop=no \
--without-xmlto \
--with-pic \
--disable-static \
--disable-acfb \
--disable-ccfb \
--disable-mcfb \
--disable-xinerama \
--disable-xf86misc \
--disable-xorgcfg \
--disable-record \
--disable-dmx \
--disable-xnest \
--enable-xvfb \
--enable-composite \
--without-dtrace \
--with-int10=x86emu \
--sysconfdir=/etc/X11 \
--localstatedir=/var \
--with-fontdir=${datadir}/fonts/X11 \
--with-xkb-output=/var/lib/xkb \
ac_cv_file__usr_share_sgml_X11_defs_ent=no \
"
PACKAGECONFIG ??= "udev ${@base_contains('DISTRO_FEATURES', 'opengl', 'dri dri2 glx', '', d)}"
PACKAGECONFIG[udev] = "--enable-config-udev,--disable-config-udev,udev"
PACKAGECONFIG[dri] = "--enable-dri,--disable-dri,glproto virtual/mesa xf86driproto"
PACKAGECONFIG[dri2] = "--enable-dri2,--disable-dri2,dri2proto"
PACKAGECONFIG[glx] = "--enable-glx --enable-glx-tls,--disable-glx,glproto virtual/libgl virtual/libx11"
*********************************************************************************************************************
I don't know how to check what type of xserver (udev, dri, dri2, glx) is built by default...
Of course, I can provide any other necessary information. I will be really appreciate for any advices!
Thanks in advance!
Hi Konstantin,
please post this to meta-fsl-arm mailing list, so that someone familiar with xserver
could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
chip
I guess that my problem is closely related to vivante xorg driver for freescale SabreSD. However, I will follow your advice! Thanks!
P.S. By the way, how I can use the common mesa driver for Xorg instead of vivante? On this stage I do not need a gpu acceleration so it can be a workaround.
So, today I have completely rebuilt my image with the master branch (fsl-image-multimedia-full) and that damn error "ortp-error-Could not find suitable format or Xv port to work with." has gone! However, I still can't see the self view via linphone! Moreover, it crashes... And now it seems like problem in the mxc_v4l2 driver.
Here is the log message from linphone:
root@imx6qsabresd:~# linphonec -V -d 3
INFO: no logfile, logging to stdout
ortp-message-Using (r/w) config information from /home/root/.linphonerc
ortp-message-Initializing LinphoneCore 3.6.1
ortp-message-oRTP-0.22.0 initialized.
ortp-message-assigning PCMU/8000 payload type number 0
ortp-message-assigning GSM/8000 payload type number 3
ortp-message-assigning PCMA/8000 payload type number 8
ortp-message-assigning speex/8000 payload type number 110
ortp-message-assigning speex/16000 payload type number 111
ortp-message-assigning speex/32000 payload type number 112
ortp-message-assigning telephone-event/8000 payload type number 101
ortp-message-assigning G722/8000 payload type number 9
ortp-message-assigning H263/90000 payload type number 34
ortp-message-assigning theora/90000 payload type number 97
ortp-message-assigning H263-1998/90000 payload type number 98
ortp-message-assigning MP4V-ES/90000 payload type number 99
ortp-message-assigning H264/90000 payload type number 102
ortp-message-assigning VP8/90000 payload type number 103
ortp-message-assigning x-snow/90000 payload type number 96
ortp-message-assigning iLBC/8000 payload type number 100
ortp-message-assigning AMR/8000 payload type number 104
ortp-message-assigning AMR-WB/16000 payload type number 105
ortp-message-assigning 1015/8000 payload type number 106
ortp-message-assigning G726-16/8000 payload type number 107
ortp-message-assigning G726-24/8000 payload type number 108
ortp-message-assigning G726-32/8000 payload type number 109
ortp-message-assigning G726-40/8000 payload type number 113
ortp-message-assigning AAL2-G726-16/8000 payload type number 114
ortp-message-assigning AAL2-G726-24/8000 payload type number 115
ortp-message-assigning AAL2-G726-32/8000 payload type number 116
ortp-message-assigning AAL2-G726-40/8000 payload type number 117
ortp-message-assigning SILK/8000 payload type number 118
ortp-message-assigning SILK/12000 payload type number 119
ortp-message-assigning SILK/16000 payload type number 120
ortp-message-assigning SILK/24000 payload type number 121
ortp-message-assigning G729/8000 payload type number 18
ortp-message-assigning mpeg4-generic/22050 payload type number 122
ortp-message-assigning mpeg4-generic/44100 payload type number 123
ortp-message-assigning opus/48000 payload type number 124
ortp-message-assigning 1016/8000 payload type number 1
ortp-message-assigning GSM/8000 payload type number 3
ortp-message-assigning G723/8000 payload type number 4
ortp-message-assigning LPC/8000 payload type number 7
ortp-message-assigning PCMA/8000 payload type number 8
ortp-message-assigning G722/8000 payload type number 9
ortp-message-assigning L16/44100 payload type number 10
ortp-message-assigning L16/44100 payload type number 11
ortp-message-assigning G729/8000 payload type number 18
ortp-message-assigning H261/90000 payload type number 31
ortp-message-assigning MPV/90000 payload type number 32
ortp-message-assigning H263/90000 payload type number 34
ortp-message-Mediastreamer2 2.9.1 (git: 2.9.1) starting.
ortp-message-ms_base_init() done
ortp-message-Registering all soundcard handlers
ortp-message-Card 'ALSA: default device' added
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_frimx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
eescale_build/tmp/work/cortexa9hfimx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 0
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/control/control.c:953:(snd_ctl_open_noupdate) Invalid CTL default:0
ortp-warning-Could not attach mixer to card: Invalid argument
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/aERROR: v4l2 capture: slave not found!
lsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 0
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/pcm/pcm.c:2239:(snd_pcm_open_noupdate) Unknown PCM default:0
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 0
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/pcm/pcm.c:2239:(snd_pcm_open_noupdate) Unknown PCM default:0
ortp-warning-Strange, sound card wm8962-audio does not seems to be capable of anything, retrying with plughw...
ortp-message-Card 'ALSA: wm8962-audio' added
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 1
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/control/control.c:953:(snd_ctl_open_noupdate) Invalid CTL default:1
ortp-warning-Could not attach mixer to card: Invalid argument
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 1
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/pcm/pcm.c:2239:(snd_pcm_open_noupdate) Unknown PCM default:1
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/conf.c:4694:(snd_config_expand) Unknown parameters 1
ALSA lib /mnt/Data/Linux_arm/fsl-release-bsp/my_freescale_build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/alsa-lib/1.0.27.2-r0/alsa-lib-1.0.27.2/src/pcm/pcm.c:2239:(snd_pcm_open_noupdate) Unknown PCM default:1
ortp-warning-Strange, sound card imx-hdmi-soc does not seems to be capable of anything, retrying with plughw...
ortp-warning-Strange, sound card imx-hdmi-soc seems totally unusable.
ortp-message-Card 'ALSA: imx-hdmi-soc' added
ortp-message-Card 'PulseAudio: default' added
ortp-message-New PulseAudio context state: PA_CONTEXT_CONNECTING
ortp-message-New PulseAudio context state: PA_CONTEXT_FAILED
ortp-message-Registering all webcam handlers
ortp-message-Webcam V4L2: /dev/video1 added
ortp-message-Webcam StaticImage: Static picture added
ortp-message-ms_voip_init() done
ortp-message-Loading ms plugins from [/usr/lib/mediastreamer/plugins]
ortp-message-Cannot open directory /usr/lib/mediastreamer/plugins: No such file or directory
ortp-message-Cannot open directory /usr/lib/liblinphone/plugins: No such file or directory
ortp-message-linphone_core_set_playback_gain_db(): no active call.
ortp-message-linphone_core_set_mic_gain_db(): no active call.
ortp-message-MTU is supposed to be 1300, rtp payload max size will be 1240
ortp-message-Adding new codec PCMU/8000 with fmtp
ortp-message-Could not find encoder for 1016
ortp-message-Could not find decoder for 1016
ortp-message-Could not find encoder for GSM
ortp-message-Could not find decoder for GSM
ortp-message-Could not find encoder for G723
ortp-message-Could not find decoder for G723
ortp-message-Could not find encoder for LPC
ortp-message-Could not find decoder for LPC
ortp-message-Adding new codec PCMA/8000 with fmtp
ortp-message-Adding new codec G722/8000 with fmtp
ortp-message-Adding new codec L16/44100 with fmtp
ortp-message-Adding new codec L16/44100 with fmtp
ortp-message-Could not find encoder for G729
ortp-message-Could not find decoder for G729
ortp-message-Could not find encoder for iLBC
ortp-message-Could not find decoder for iLBC
ortp-message-Could not find encoder for telephone-event
ortp-message-Could not find decoder for telephone-event
ortp-message-Could not find encoder for AMR
ortp-message-Could not find decoder for AMR
ortp-message-Could not find encoder for AMR-WB
ortp-message-Could not find decoder for AMR-WB
ortp-message-Could not find encoder for 1015
ortp-message-Could not find decoder for 1015
ortp-message-Could not find encoder for G726-16
ortp-message-Could not find decoder for G726-16
ortp-message-Could not find encoder for G726-24
ortp-message-Could not find decoder for G726-24
ortp-message-Could not find encoder for G726-32
ortp-message-Could not find decoder for G726-32
ortp-message-Adding new codec speex/8000 with fmtp vbr=on
ortp-message-Adding new codec speex/16000 with fmtp vbr=on
ortp-message-Adding new codec speex/32000 with fmtp vbr=on
ortp-message-Could not find encoder for G726-40
ortp-message-Could not find decoder for G726-40
ortp-message-Could not find encoder for AAL2-G726-16
ortp-message-Could not find decoder for AAL2-G726-16
ortp-message-Could not find encoder for AAL2-G726-24
ortp-message-Could not find decoder for AAL2-G726-24
ortp-message-Could not find encoder for AAL2-G726-32
ortp-message-Could not find decoder for AAL2-G726-32
ortp-message-Could not find encoder for AAL2-G726-40
ortp-message-Could not find decoder for AAL2-G726-40
ortp-message-Could not find encoder for SILK
ortp-message-Could not find decoder for SILK
ortp-message-Could not find encoder for SILK
ortp-message-Could not find decoder for SILK
ortp-message-Could not find encoder for SILK
ortp-message-Could not find decoder for SILK
ortp-message-Could not find encoder for SILK
ortp-message-Could not find decoder for SILK
ortp-message-Could not find encoder for mpeg4-generic
ortp-message-Could not find decoder for mpeg4-generic
ortp-message-Could not find encoder for mpeg4-generic
ortp-message-Could not find decoder for mpeg4-generic
ortp-message-Could not find encoder for opus
ortp-message-Could not find decoder for opus
ortp-message-Could not find encoder for H261
ortp-message-Could not find decoder for H261
ortp-message-Could not find encoder for MPV
ortp-message-Could not find decoder for MPV
ortp-message-Could not find encoder for H263
ortp-message-Could not find decoder for H263
ortp-message-Could not find encoder for x-snow
ortp-message-Could not find decoder for x-snow
ortp-message-Adding new codec theora/90000 with fmtp
ortp-message-Could not find encoder for H263-1998
ortp-message-Could not find decoder for H263-1998
ortp-message-Could not find encoder for MP4V-ES
ortp-message-Could not find decoder for MP4V-ES
ortp-message-Could not find encoder for H264
ortp-message-Could not find decoder for H264
ortp-message-Could not find encoder for VP8
ortp-message-Could not find decoder for VP8
ortp-message-getaddrinfo returned the following addresses:
ortp-message-0.0.0.0 port 5060
ortp-message-eXosip: Reseting timer to 10s before waking up!
Ready
linphonec> ortp-error-Error in connect: Network is unreachable
ortp-message-Setting video size 352x288
ortp-message-Driver is mxc_v4l2
ortp-message-v4l2: trying 352x288
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 352x288
ortp-message-v4l2: trying 320x240
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 320x240
ortp-message-v4l2: trying 176x144
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 176x144
ortp-message-Could not find any combination of resolution/pixel-format that works !
ortp-message-Driver is mxc_v4l2
ortp-message-v4l2: trying 352x288
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 352x288
ortp-message-v4l2: trying 320x240
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 320x240
ortp-message-v4l2: trying 176x144
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-message-VIDIOC_TRY_FMT: Invalid argument
ortp-error-Could not find supported pixel format for 176x144
ortp-message-Could not find any combination of resolution/pixel-format that works !
Segmentation fault
Any suggestions?
Hi Konstantin,
linphone 3.7.0 is very special software,
not sure that it can be supported here.
please post this to meta-fsl-arm mailing list, so that someone familiar with it
could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
chip