Length of ADDR13 line in i.MX6 ULL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Length of ADDR13 line in i.MX6 ULL-EVK

Jump to solution
656 Views
victorpecanins
Contributor II

Hello,

I am developing custom board based on i.MX6 ULL.

I was checking the DDRrouting in the layout files of the MCIMX6ULL-EVK (Allegro board layout files publicly available from NXP website).

I noticed the ADDR13 line has an unusually big length of 1411.4173 mils (measured with Allegro). The average length of the address lines is 1386.5559 mils, and other tracks do not deviate more than 10 mils from this value.

To my understanding, the ADDR13 is violating the design rules of the document IMX6ULHDG "Hardware Development Guide for the i.MX 6UltraLite Applications Processor", page 25, table 22: "Match the signals ± 25 mils."

My question is: This extra length is intentional? In my design, can I make this track shorter and close to the average of the rest of the lanes of this address bus? Or should I make it longer, to overcome an undocumented issue?

Best Regards,

Tags (1)
0 Kudos
Reply
1 Solution
555 Views
igorpadykov
NXP Employee
NXP Employee

Hi Victor

there are no special routing issues/rules for ADDR13 and it should follow

Hardware Development Guide recommendations. As EVK was developed before

processor documentation was fully developed, its layout may differ from Guide.

Recommendation for customers is to follow formal document given in

Hardware Development Guide recommendations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
556 Views
igorpadykov
NXP Employee
NXP Employee

Hi Victor

there are no special routing issues/rules for ADDR13 and it should follow

Hardware Development Guide recommendations. As EVK was developed before

processor documentation was fully developed, its layout may differ from Guide.

Recommendation for customers is to follow formal document given in

Hardware Development Guide recommendations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------