When I set the LVDS resolution on u-boot, LVDS driver can automatically calculate timings parameters.
Could you please provide the formula of calculating timings?
For example:
I set LVDS resolution (1280*1024) on u-boot. After booting the device, type "fbset" command:
mode "1280x1024-60"
# D: 109.004 MHz, H: 63.670 kHz, V: 59.897 Hz
geometry 1280 1024 1280 1024 16
timings 9174 216 80 3 29 136 7
vsync high
rgba 5/11,6/5,5/0,0/0
endmode
LVDS driver can automatically calculate timings parameters (9174 216 80 3 29 136 7).
Could you please provide the formula of calculating timings?
Thanks.
Best Regards,
Alex
Hi charles
for new lcd timings configuration one can look at
Chapter 18 Connecting an LVDS Panel i.MX53 System Development User’s Guide.
http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf
However I do not think that u-boot-2009.08 automatically calculate timings,
probably it adjusts it to most close value.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------