Hello Community
In the Datasheet of i.MX6SoloX,there is description as bellow:
--------------------
Displays—Total two interfaces available.
— One Parallel 24-bit display port, up to dual WXGA at 60 Hz
— LVDS serial port—One port up to 85 MP/sec (for example, WXGA at 60 Hz)
-------------------
Question:
Q1)
According to IMX6SXRM.pdf, there are two Parallel 24-bit display port.
It seems that the datasheet made a mistake, right?
Q2)
I want to know the exact max pixclk of parallel display port.(The datasheet just says up to dual WXGA at 60 Hz).
Thank you!
ZongbiaoLiao
A1. Yes, you are right, the i.MX6SoloX Data Sheet document is incorrect in that.
Actually, the i.MX6SoloX processor has two parallel LCD interfaces.
A2. As per the Data Sheet document, the maximum pixel clock frequency of the LCD interface module is 150MHz.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------