LCD doesn't work (fsl,mxc_sdc_fb)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD doesn't work (fsl,mxc_sdc_fb)

Jump to solution
2,235 Views
michaellosert
Contributor I

I'm currently trying to get a LCD display to work on a custom imx6dl.

The fsl,mxc_sdc_fb framebuffer driver is definitely compiled and also loads. But the probe function is never called.

/ {

    aliases {

        mxcfb2 = &mxcfb3;

    };

    mxcfb3: fb@0 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "lcd";

        interface_pix_fmt = "RGB666";

        default_bpp = <18>;

        int_clk = <0>;

        late_init = <0>;

        status = "okey";

    };

    lcd@0 {

        compatible = "fsl,lcd";

        ipu_id = <0>;

        disp_id = <0>;

        default_ifmt = "RGB666";

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_ipu1>;

        status = "okay";

    };

....

};

...

&mxcfb3 {

    status = "okey";

};

that's what I have in the device tree.

The LCD is at ipu1_di0_disp0.

I also tried booting with

setenv bootargs "video=mxcfb2:dev=lcd,CLAA-WVGA,if=RGB666 console=${console},115200 root=${mmcroot}";

mxc_sdc_fb creates no output in the kernel log at all while fsl,imx6dl-epdc does.

kernel log:

https://paste.debian.net/313932/

I know for sure that it can't be an hwardware issue because the display works in u-boot.

I'm forced to use linux-imx (3.14) because it's part of yocto fido (1.8) and I need meta-qt5 support.

Labels (3)
Tags (2)
0 Kudos
1 Solution
1,362 Views
michaellosert
Contributor I

OK so I got it working by removing

     default_bpp = <18>;

and adding

     mode_str ="MY-DISPLAY";

instead.

I also added the displays settings to lcdif_modedb.

{

  /* 320x240 @ 60 Hz , pixel clk @ 6.5MHz */

  "MY-DISPLAY", 60, 320, 240, 153846, 68, 20, 18, 4, 1, 1,

  0,

  FB_VMODE_NONINTERLACED,

  0

},}

see also

How do I configure a 320x240 LCD in the Device Tree for i.MX6 Solo?

View solution in original post

0 Kudos
1 Reply
1,363 Views
michaellosert
Contributor I

OK so I got it working by removing

     default_bpp = <18>;

and adding

     mode_str ="MY-DISPLAY";

instead.

I also added the displays settings to lcdif_modedb.

{

  /* 320x240 @ 60 Hz , pixel clk @ 6.5MHz */

  "MY-DISPLAY", 60, 320, 240, 153846, 68, 20, 18, 4, 1, 1,

  0,

  FB_VMODE_NONINTERLACED,

  0

},}

see also

How do I configure a 320x240 LCD in the Device Tree for i.MX6 Solo?

0 Kudos