I'm trying to get a HX8369A based lcd to display 18-bit parallel RGB. I've got it working but the colors look terrible. A lot of pixels just go to green like the color data is incorrect. I've tried a variety of timings but it doesn't help.
Does this seem like a timing issue? Is the software giving bad color data? Could my LCD be expecting color data in a slightly different format?
I'm using an IMX6S based RIoTboard which only has DISP_DAT0 - DISP0_DAT17 accessible on the header so I can't use 24 bits. Kernel 3.0.35, Android 4.3.
Boot Arguments:
setenv bootargs console=ttymxc1,115200 init=/init video=mxcfb0:dev=lcd,CLAA-WVGA@60,bpp=18,if=RGB666 video=mxcfb1:off fbmem=10M vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale
Timing in mxc_lcdif.c:
static struct fb_videomode lcdif_modedb[] = {
{
"CLAA-WVGA", 60, 480, 800, KHZ2PICOS(25000), 5, 5, 2, 2, 5, 2,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,
},
//...
}
FB configuration in board-mx6solo_RIoTboard.c:
static struct fsl_mxc_lcd_platform_data lcdif_data = {
.ipu_id = 0,
.disp_id = 0,
.default_ifmt = IPU_PIX_FMT_RGB666,
};
//...
static struct ipuv3_fb_platform_data RIoTboard_fb_data[] = {
{
.disp_dev = "lcd",
.interface_pix_fmt = IPU_PIX_FMT_RGB666,
.mode_str = "CLAA-WVGA",
.default_bpp = 18,
.int_clk = false,
},
//...
}
Pin Muxing in board-mx6solo_RIoTboard.h:
/* DISPLAY */
MX6DL_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK,
MX6DL_PAD_DI0_PIN15__IPU1_DI0_PIN15, /* DE */
MX6DL_PAD_DI0_PIN2__IPU1_DI0_PIN2, /* HSync */
MX6DL_PAD_DI0_PIN3__IPU1_DI0_PIN3, /* VSync */
//MX6DL_PAD_DI0_PIN4__IPU1_DI0_PIN4, /* Contrast not connected*/
MX6DL_PAD_DISP0_DAT0__IPU1_DISP0_DAT_0,
MX6DL_PAD_DISP0_DAT1__IPU1_DISP0_DAT_1,
MX6DL_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2,
MX6DL_PAD_DISP0_DAT3__IPU1_DISP0_DAT_3,
MX6DL_PAD_DISP0_DAT4__IPU1_DISP0_DAT_4,
MX6DL_PAD_DISP0_DAT5__IPU1_DISP0_DAT_5,
MX6DL_PAD_DISP0_DAT6__IPU1_DISP0_DAT_6,
MX6DL_PAD_DISP0_DAT7__IPU1_DISP0_DAT_7,
MX6DL_PAD_DISP0_DAT8__IPU1_DISP0_DAT_8,
MX6DL_PAD_DISP0_DAT9__IPU1_DISP0_DAT_9,
MX6DL_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10,
MX6DL_PAD_DISP0_DAT11__IPU1_DISP0_DAT_11,
MX6DL_PAD_DISP0_DAT12__IPU1_DISP0_DAT_12,
MX6DL_PAD_DISP0_DAT13__IPU1_DISP0_DAT_13,
MX6DL_PAD_DISP0_DAT14__IPU1_DISP0_DAT_14,
MX6DL_PAD_DISP0_DAT15__IPU1_DISP0_DAT_15,
MX6DL_PAD_DISP0_DAT16__IPU1_DISP0_DAT_16,
MX6DL_PAD_DISP0_DAT17__IPU1_DISP0_DAT_17,
Does 18-bit color just look this bad?
已解决! 转到解答。
I think I've nearly got it!
SteveRathjen was correct about adding a 330 Ohm resistor inline with the CLK signal. That improved the image dramatically.
Then using the patches louiskoziarz recommended as a guide I changed the CLK pin strength, I bumped the control type up to PAD_CTL_DSE_240ohm and have a nearly perfect image. Although there are still a few errant blue pixels.
I have asked my coworker to add pads for inline resistors on all the display lines for the next version of our board. I'm sure that tuning those values and the pin strengths will help us get a perfect image.
Thanks to everyone for their help!
I think I've nearly got it!
SteveRathjen was correct about adding a 330 Ohm resistor inline with the CLK signal. That improved the image dramatically.
Then using the patches louiskoziarz recommended as a guide I changed the CLK pin strength, I bumped the control type up to PAD_CTL_DSE_240ohm and have a nearly perfect image. Although there are still a few errant blue pixels.
I have asked my coworker to add pads for inline resistors on all the display lines for the next version of our board. I'm sure that tuning those values and the pin strengths will help us get a perfect image.
Thanks to everyone for their help!
Hi Marvin,
Could you please help me here? What all things I need to verify to get LCD working?
Innolux LCD brignup on i.MX6 Solo Sabre based board
Thanks & Regards,
Vikash
Luke,
I was having a VERY similar problem with an RGB666 LCD and an iMX6Solo. This was using a Nitrogen6X SOM from Boundary and their 800x480 LCD.
Eric Nelson from Boundary was extremely helpful and tackled the issue. He's committed two patches to fix the problem for me and it works GREAT. You might want to give these a try, if not directly pulling them into your kernel then at least you can get the spirit of what is changing here.
Patch 1 corrects the drive strength on the LCD lines. Eric notes this is normally done in the bootloader but makes sure they're set again in the kernel:
Patch 2 corrects the LCD pixel clock polarity. According to Eric it was being reset during mode changes.
ipu_disp: preserve display clock polarity · a885ae0 · boundarydevices/linux-imx6 · GitHub
I'm sure Eric would show up here soon and give the same info, I'm paying back the favor by saving him the keystrokes...
Okay I've made those changes to my uboot, kernel and lcd driver. Alas it does not seem to have solved my problem. Certain colours still won't display correctly.
But at least I won't have to worry about that problem later! :smileylaugh:
Do you have series resistors in line with the LCD signals? Especially the clock? I had 33 ohm on all and had similar noise on display. I found a 330 ohm on the clock line fixed it.
Also make sure your boot cmd has something like "video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB666" for 18 bit.
Steve
My board (Embest Tech RIoTboard) doesn't have any inline resistors on any of the lines.
I took a look at the schematic for the Sabre Lite. It doesn't have any resistors on the data lines but the schematic shows a mystery resistor on the CLK line. Is it just a 0 Ohms resistor? Should I have a resistor on my clock line?
The SabreSD has these 33 ohm resistors. I included them on my custom board, but changed CLK resistor to 330 ohm - the noise on the display looked VERY similar to what you see with 33 ohm on the CLK. I'm using a display with a HX8264 and 24bit. The noise when connecting the LCD to the SabreSD was 10x compared to my custom board, but I had several "adapters" to get the LCD connected to the SabreSD.
I'd seriously consider trying a resistor 33-330ohm on the CLK line if it's not too much hassle.
Hope that helps!
Steve
It's a new LCD from Microtips. It uses the HX8369A controller IC. This is the initialization code I was given. I'm bit banging the SPI over GPIOS.
Yes that's how I have them wired up.
I saw another post where some said that in the boot arguments should have bpp = 32 instead of bpp = 18. I changed that and it helped most of the image but there are still certain colors it refuses to display properly.
When I display the following image...
...certain colors just appear as green.
That leads me to believe it's some sort of encoding problem, rather than a timing problem.
I have a linux image provided by the vendor however I don't know what the pin muxing is. Is there a way to set the muxing from user space?
The vendor hasn't supplied the source code and I've only been setting pin muxes with define statements. Also this kernel pre-dates device trees.
Most likely the pins should be setup for LCDs. One way to confirm them is to use the devregs utility and read the mux settings from user space.
http://boundarydevices.com/i-mx5x-device-register-access/
Note: link is for imx5 but see github link in there for imx6 code.
Well it turns out the vendor has put up linux source since I last checked. I built an image configured for my LCD but found that I still have the same colour issues. This distribution is using the same kernel and drivers as the Android image did.
So I can at least rule out the OS as the source of the problem. It's either in the kernel video drivers, the hardware lines or the LCD initialization settings.