L4.1.15_1.1.0_ga-mfg-tools for i.MX6ULEVK board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L4.1.15_1.1.0_ga-mfg-tools for i.MX6ULEVK board

954 Views
yuuki
Senior Contributor II

Dear all,

We removed the SD card socket of the i.MX6UL EVK board.

And we attached eMMC device.

We tried QSPI boot and eMMC boot.

  • For QSPI boot

We wrote in Image using mfgtool2-yocto-mx-evk-qspi-nor-n25q256a.vbs.

Writing was completed, but we cannot access eMMC.

========================================

mmc info

Card did not respond to voltage select!

========================================

<Question>

Is the QSPI Boot image that is available for access to eMMC included in this Tool?

Would you tell me the file name if there is it?

  • For eMMC boot

We wrote in Image using mfgtool2-yocto-mx-evk-sdcard-sd2.vbs.

Writing was completed, however evk board does not boot from eMMC.

<Question>

Would you tell me the image file that eMMC boot is tested on evk board?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Reply

476 Views
Yuri
NXP Employee
NXP Employee

Hello,

    First, please double check BOOT_CFG configuration, if it is suitable

to boot uSDHC2.
     Also, please try files with  "imx6ul-14x14-ddr3-arm2-emmc" postfix

from the demo images.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply