Kernel panic when login on iMX6 (Micron Nand + ubifs)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel panic when login on iMX6 (Micron Nand + ubifs)

Jump to solution
1,610 Views
abrahim
Contributor III

Hello,

I'm building a buildroot BSP for a iMX6 solo core :

  • U-Boot 2020.04
  • Linux version 5.10.9
  • Buildroot 2022.11-1380-g1613273542

 

When I boot and login, I have a long kernel panic message. It seems to be due to the filesystem :

 

Buildroot login: root
[ 16.615654] 8<--- cut here ---
[ 16.618754] Unable to handle kernel paging request at virtual address 0124d494
[ 16.626708] 8<--- cut here ---
[ 16.629793] Unable to handle kernel NULL pointer dereference at virtual address 00000003
[ 16.637996] pgd = 302756ad
[ 16.640719] [00000003] *pgd=00000000
[ 16.644353] Internal error: Oops: 805 [#1] PREEMPT SMP ARM
[ 16.649856] Modules linked in: imx_vdoa
[ 16.653720] CPU: 0 PID: 257 Comm: systemd Not tainted 5.10.9 #39
[ 16.659744] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 16.666300] PC is at __insert_inode_hash+0x7c/0x94
[ 16.671099] LR is at __insert_inode_hash+0x5c/0x94
[ 16.675903] pc : [<80272dc8>] lr : [<80272da8>] psr: a00b0013
[ 16.682185] sp : 8296bc78 ip : 0003df3f fp : 8429e198
[ 16.687421] r10: 8444a678 r9 : 00000048 r8 : dabf7878
[ 16.692650] r7 : 844ba068 r6 : dab99000 r5 : 844ba0a0 r4 : 00017a1e
[ 16.699184] r3 : ffffffff r2 : 00000001 r1 : 00000000 r0 : 844ba068
[ 16.705727] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 16.712879] Control: 10c5387d Table: 1288c059 DAC: 00000051
[ 16.718638] Process systemd (pid: 257, stack limit = 0xa7b5c38d)
[ 16.724660] Stack: (0x8296bc78 to 0x8296c000)
[ 16.729030] bc60: 00000000 8429e000
[ 16.737233] bc80: 8444a660 82671000 844ba000 803efcf8 00000000 00000000 827a70c0 00000000
[ 16.745432] bca0: 00100050 00000000 00000180 000001d8 000000a0 8444a678 8444a68c 00000008
[ 16.753630] bcc0: 00000000 00000000 00000000 00000000 00000000 ba1e2c76 8296bd70 803efb34
[ 16.761829] bce0: 8444a660 841d26e8 00000000 8296bd70 8296be18 827a70c0 8120fec4 80266750
[ 16.770027] bd00: 00000001 00000005 82772000 80249ecc 00000040 000280c2 00000001 00000000
[ 16.778217] bd20: 8429e000 00008180 00000040 8296a000 00000001 ffffffec 00000000 8296bd3c
[ 16.786408] bd40: 8296bd3c ba1e2c76 00000000 000280c2 8296be18 00000000 8139ddb8 00000000
[ 16.794608] bd60: 829b9200 00000000 8296a000 8026866c 826943d0 841d26e8 61f080fd 00000008
[ 16.802800] bd80: 82a00010 82713d04 00000000 8024bac0 8429e000 00000700 00000002 000008de
[ 16.810999] bda0: 000004ac 00000000 00000000 00000000 8296bdb4 8296a000 8296bdc8 0008b420
[ 16.819197] bdc0: 82a00000 80242130 8296bdd0 00000000 82a00000 ba1e2c76 ffffffec 000280c2
[ 16.827396] bde0: 00000008 82a00000 00000000 829b9200 ffffff9c 00000000 82a041ed 80267034
[ 16.835587] be00: 000280c2 ba1e2c76 000280c2 82a00000 00000180 80252920 000280c2 828c8180
[ 16.843777] be20: 00000006 00000700 00000000 ba1e2c76 828c4300 82938a00 812df550 802c7a20
[ 16.851968] be40: 8c01818f ffefe0c8 8c01818f 801164c4 00000000 00000000 00000000 00000000
[ 16.860159] be60: 828c4f00 828c4300 00000000 829b9200 00000008 00000080 826dfd20 80242130
[ 16.868356] be80: 8296be88 8296a000 826dfd20 00000000 826ff6c0 00000000 00000000 00000000
[ 16.876555] bea0: 8296bea0 8296bea0 8296bf60 8296bfb0 00000000 ffffffff 000000cd 00000000
[ 16.884752] bec0: 00000000 00000000 00000000 00000000 7ed860ec ba1e2c76 00000001 0000000a
[ 16.892944] bee0: 8296a000 400004d8 8294ca80 8296bf60 826c9180 8296a000 0000000a 801401a4
[ 16.901135] bf00: 00000000 8296bf4c 826943c0 81395028 8294ca80 8296a000 8296bfb0 76a64d28
[ 16.909326] bf20: fffffe30 8296bf4c 5ac3c35a 81204f8c 00000000 8010984c 0000000b 76a64d2c
[ 16.917516] bf40: 8296bf64 8013f904 00000000 00000101 0000000b 8296a000 ffffe000 80140e7c
[ 16.925713] bf60: 0000000b 00000000 00000000 00000101 00000000 00000000 00000000 00000000
[ 16.933913] bf80: 00000000 ba1e2c76 0000000b 0000000b 00000000 7ed85ce0 00000025 80100264
[ 16.942102] bfa0: 8296a000 00000025 7ed860ec 801000cc 00000000 0000000b 00000000 00000000
[ 16.950300] bfc0: 0000000b 00000000 7ed85ce0 00000025 7ed85c48 7ed85c4c 00000001 7ed860ec
[ 16.958490] bfe0: 00442d1c 7ed85b94 0042e318 76a64d2c 000b0010 00000101 00000000 00000000
[ 16.966703] [<80272dc8>] (__insert_inode_hash) from [<803efcf8>] (ubifs_create+0x1c4/0x210)
[ 16.975090] [<803efcf8>] (ubifs_create) from [<80266750>] (path_openat+0x4d4/0xd3c)
[ 16.982777] [<80266750>] (path_openat) from [<8026866c>] (do_filp_open+0x70/0x120)
[ 16.990370] [<8026866c>] (do_filp_open) from [<80252920>] (filp_open+0x118/0x1a4)
[ 16.997888] [<80252920>] (filp_open) from [<802c7a20>] (do_coredump+0xde4/0x11a8)
[ 17.005393] [<802c7a20>] (do_coredump) from [<801401a4>] (get_signal+0x138/0x7e4)
[ 17.012908] [<801401a4>] (get_signal) from [<8010984c>] (do_work_pending+0x110/0x594)
[ 17.020760] [<8010984c>] (do_work_pending) from [<801000cc>] (slow_work_pending+0xc/0x20)
[ 17.028958] Exception stack(0x8296bfb0 to 0x8296bff8)
[ 17.034017] bfa0: 00000000 0000000b 00000000 00000000
[ 17.042209] bfc0: 0000000b 00000000 7ed85ce0 00000025 7ed85c48 7ed85c4c 00000001 7ed860ec
[ 17.050408] bfe0: 00442d1c 7ed85b94 0042e318 76a64d2c 000b0010 00000101
[ 17.057047] Code: f57ff05b e1a00007 e7865104 e3530000 (15835004)
[ 17.063202] ---[ end trace 536dee15ce23eef6 ]---
[ 17.067843] note: systemd[257] exited with preempt_count 2
[ 17.073431] pgd = 658dd51f
[ 17.076155] [0124d494] *pgd=00000000
[ 17.079745] Internal error: Oops: 5 [#2] PREEMPT SMP ARM
[ 17.085070] Modules linked in: imx_vdoa
[ 17.088934] CPU: 0 PID: 176 Comm: systemd-journal Tainted: G D 5.10.9 #39
[ 17.097044] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 17.103589] PC is at __d_lookup_rcu+0x64/0x184
[ 17.108041] LR is at lookup_fast+0x44/0x184
[ 17.112238] pc : [<8027217c>] lr : [<80262e54>] psr: 200f0013
[ 17.118509] sp : 827c7d30 ip : 239b8cba fp : 00010001
[ 17.123738] r10: d0d0d0d0 r9 : 239b8cba r8 : 00000003
[ 17.128978] r7 : 00000003 r6 : 82a01014 r5 : 841d26e8 r4 : 0124d498
[ 17.135510] r3 : 827c7e80 r2 : 00ffffff r1 : ffffffff r0 : dac19000
[ 17.142052] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 17.149193] Control: 10c5387d Table: 12804059 DAC: 00000051
[ 17.154957] Process systemd-journal (pid: 176, stack limit = 0xa8831ba8)
[ 17.161675] Stack: (0x827c7d30 to 0x827c8000)
[ 17.166047] 7d20: 812dbe60 827c7d68 00ffffff 827ee480
[ 17.174238] 7d40: 00000001 82a01015 827c7e78 827c7d94 827c7d98 841d26e8 00000018 d0d0d0d0
[ 17.182429] 7d60: 00010001 80262e54 000000c4 ba1e2c76 82a01015 00000000 827c7e78 00000002
[ 17.190629] 7d80: 2f2f2f2f 80265b60 8429e000 00000081 00000000 827c7e78 2f2f2f2f ba1e2c76
[ 17.198828] 7da0: 827a79c0 82a01015 00000000 fefefeff 827c7e78 2f2f2f2f 00000018 80265f34
[ 17.207030] 7dc0: 00000000 61c88647 827c7e78 00000041 82a01010 80263b00 827c7e78 ba1e2c76
[ 17.215230] 7de0: 82a01010 ffffe000 82a01010 00000001 ffffff9c 827c7e78 827c7f30 827a79c0
[ 17.223430] 7e00: ffffffff 80266328 827c7f60 000000ad 7ef20674 7ef20690 7ef20710 809aa088
[ 17.231621] 7e20: 820b2000 80151f0c dad20400 00000000 00000041 827c6000 7ef2066c 00000001
[ 17.239814] 7e40: 827c7ef4 827c7ef4 00000008 ba1e2c76 00000051 82a01000 827c7f30 00000001
[ 17.248013] 7e60: ffffff9c 80100264 827c6000 00000142 ffffffff 8026866c 826943d0 841d26e8
[ 17.256212] 7e80: 239b8cba 00000003 82a01011 00000000 826943d0 841d26e8 8429e000 00000051
[ 17.264405] 7ea0: 00000002 000008de 000004ac 00000000 00000000 00000000 827c7ebc 0008b40c
[ 17.272604] 7ec0: 82a01000 80242130 827c7ed0 00000000 82a01000 ba1e2c76 827a70c0 00000015
[ 17.280802] 7ee0: 82048200 827eeb00 00000000 82a01000 00000000 00000002 ffffff9c 82a01000
[ 17.289002] 7f00: 00000000 827c7f60 ffffff9c ba1e2c76 82a01000 00000015 827c7f60 80253c98
[ 17.297201] 7f20: fffffe30 80100264 bcba855e 00000003 00020802 ba1e0000 00000006 00000100
[ 17.305400] 7f40: 00000001 ba1e2c76 80100264 ffffff9c 01c0c950 01c0c950 00000142 802540f0
[ 17.313600] 7f60: 000a0802 00000000 00000000 00000000 00000000 00000000 000a0802 00000000
[ 17.321793] 7f80: 00000000 00000000 00000000 00000000 249b5bb6 ba1e2c76 40000040 000a0802
[ 17.329991] 7fa0: 00000000 80100060 000a0802 00000000 ffffff9c 01c0c950 000a0802 00000000
[ 17.338182] 7fc0: 000a0802 00000000 01c0c950 00000142 7ef201df 7ef20370 01bfc790 ffffffff
[ 17.346380] 7fe0: 00000000 7ef20150 00000000 76ca2140 800f0010 ffffff9c 00000000 00000000
[ 17.354586] [<8027217c>] (__d_lookup_rcu) from [<80262e54>] (lookup_fast+0x44/0x184)
[ 17.362357] [<80262e54>] (lookup_fast) from [<80265b60>] (walk_component+0x38/0x1d8)
[ 17.370127] [<80265b60>] (walk_component) from [<80265f34>] (link_path_walk.part.0.constprop.0+0x234/0x358)
[ 17.379885] [<80265f34>] (link_path_walk.part.0.constprop.0) from [<80266328>] (path_openat+0xac/0xd3c)
[ 17.389296] [<80266328>] (path_openat) from [<8026866c>] (do_filp_open+0x70/0x120)
[ 17.396891] [<8026866c>] (do_filp_open) from [<80253c98>] (do_sys_openat2+0xa0/0x15c)
[ 17.404738] [<80253c98>] (do_sys_openat2) from [<802540f0>] (sys_openat+0x9c/0xc4)
[ 17.412335] [<802540f0>] (sys_openat) from [<80100060>] (ret_fast_syscall+0x0/0x54)
[ 17.420010] Exception stack(0x827c7fa8 to 0x827c7ff0)
[ 17.425079] 7fa0: 000a0802 00000000 ffffff9c 01c0c950 000a0802 00000000
[ 17.433270] 7fc0: 000a0802 00000000 01c0c950 00000142 7ef201df 7ef20370 01bfc790 ffffffff
[ 17.441460] 7fe0: 00000000 7ef20150 00000000 76ca2140
[ 17.446529] Code: ea000002 e5944000 e3540000 0a00003b (e5141004)
[ 17.452845] ---[ end trace 536dee15ce23eef7 ]---

The Ubifs seems to mount normally :

[ 3.214389] UBIFS (ubi0:0): Mounting in unauthenticated mode
[ 3.220267] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 160
[ 3.248176] UBIFS (ubi0:0): recovery needed
[ 3.344811] UBIFS (ubi0:0): recovery completed
[ 3.349514] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 3.357051] UBIFS (ubi0:0): LEB size: 253952 bytes (248 KiB), min./max. I/O unit sizes: 4096 bytes/4096 bytes
[ 3.367047] UBIFS (ubi0:0): FS size: 298139648 bytes (284 MiB, 1174 LEBs), journal size 9404416 bytes (8 MiB, 38 LEBs)
[ 3.377789] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB)
[ 3.383680] UBIFS (ubi0:0): media format: w4/r0 (latest is w5/r0), UUID 39985E51-9058-44D8-94E7-9DB9920A1755, small LPT model
[ 3.395291] VFS: Mounted root (ubifs filesystem) on device 0:15.

And the Nand is known :

[ 1.638730] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3
[ 1.645213] nand: Micron MT29F8G08ABACAH4
[ 1.649245] nand: 1024 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224

Ubifsmount on u-boot works perfectly, I can see the file system mounted and I can load files.Here's my boot command :

bootargs=onsole=ttymxc1,115200 ubi.mtd=nandrootfs root=ubi0:rootfs rootfstype=ubifs rw mtdparts=gpmi-nand:64m(nandboot),16m(nandkernel),16m(nanddtb),16m(nandtee),-(nandrootfs)
bootcmd=nand read ${loadaddr} 0x4000000 0xc00000;nand read ${fdt_addr} 0x5000000 0x100000;if test ${tee} = yes; then nand read ${tee_addr} 0x4000000 0x400000;bootm ${tee_addr} - ${fdt_addr};else bootz ${loadaddr} - ${fdt_addr};fi

My DTS configuration :

 

pinctrl_gpmi_nand: gpminandgrp {
fsl,pins = <
MX6QDL_PAD_NANDF_CLE__NAND_CLE 0xb0b1
MX6QDL_PAD_NANDF_ALE__NAND_ALE 0xb0b1
MX6QDL_PAD_NANDF_CS0__NAND_CE0_B 0xb0b1
MX6QDL_PAD_NANDF_RB0__NAND_READY_B 0xb000
MX6QDL_PAD_NANDF_D0__NAND_DATA00 0xb0b1
MX6QDL_PAD_NANDF_D1__NAND_DATA01 0xb0b1
MX6QDL_PAD_NANDF_D2__NAND_DATA02 0xb0b1
MX6QDL_PAD_NANDF_D3__NAND_DATA03 0xb0b1
MX6QDL_PAD_NANDF_D4__NAND_DATA04 0xb0b1
MX6QDL_PAD_NANDF_D5__NAND_DATA05 0xb0b1
MX6QDL_PAD_NANDF_D6__NAND_DATA06 0xb0b1
MX6QDL_PAD_NANDF_D7__NAND_DATA07 0xb0b1
MX6QDL_PAD_SD4_CMD__NAND_RE_B 0xb0b1
MX6QDL_PAD_SD4_CLK__NAND_WE_B 0xb0b1
MX6QDL_PAD_NANDF_WP_B__NAND_WP_B 0xb0b1
>;
};

&gpmi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpmi_nand>;
/* enable at -gpmi-weim.dts due to pin conflict */
status = "okay";
nand-on-flash-bbt;
fsl,use-minimum-ecc;
};

I flash the rootfs this way :

tftp 0x18100000 rootfs.ubifs
ubi part nandrootfs
ubi remove rootfs
ubi create rootfs
ubi write 0x18100000 rootfs 0x1322000

Boot logs and kernel .config attached.

 

0 Kudos
1 Solution
1,506 Views
abrahim
Contributor III

Hi,

I upgraded the kernel to 5.15.11 and it worked. But I still don't know what was the problem.

Best regards,

Aïda

View solution in original post

0 Kudos
5 Replies
1,507 Views
abrahim
Contributor III

Hi,

I upgraded the kernel to 5.15.11 and it worked. But I still don't know what was the problem.

Best regards,

Aïda

0 Kudos
1,580 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It looks like you have to burn the zImage again since from the beginning has error and check you device tree the one you showed looks nice.

Regards

0 Kudos
1,577 Views
abrahim
Contributor III

Hello,

Can you please tell what errors ? I burned it many many times but with the same result.

Best regards,

Aïda

0 Kudos
1,573 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

The error  Unable to handle kernel paging request at virtual address 0124d494 means that is no valid kernel image, you need to rebuild or burn again the Image.

Regards

 

0 Kudos
1,532 Views
abrahim
Contributor III

Hi,

I tried to rebuild with the following command line but I had the same result :

$ make -j8 ARCH=arm CROSS_COMPILE=../../host/usr/bin/arm-linux- zImage

Sometimes the error changes to :

Unable to handle kernel NULL pointer dereference at virtual address 000000a8

mtdparts from u-boot :

=> mtdparts
Device nor0 not found!
current device is invalid, skip it and check the next one

device nand0 <gpmi-nand>, # parts = 5
#: name size offset mask_flags
0: nandboot 0x04000000 0x00000000 0
1: nandkernel 0x01000000 0x04000000 0
2: nanddtb 0x01000000 0x05000000 0
3: nandtee 0x01000000 0x06000000 0
4: nandrootfs 0x39000000 0x07000000 0

active partition: nand0,0 - (nandboot) 0x04000000 @ 0x00000000

The kernel burn commands from u-boot :

mw.b 0x18100000 0xff 0x800000
tftp 0x18100000 zImage
nand erase.part nandkernel
nand write 0x18100000 nandkernel 0x800000

NB : the kernel is loaded so the magic is correct, isn't it ?

0 Kudos