Hello,
I able to configure the Ubuntu machine and build the images using Yocto. But now I would like to modify the kernel configuration and build the kernel with that configuration. I read somewhere that Yocto uses the kernel configuration file "<build_dir>/../sources/meta-fsl-arm/recipes-kernel/linux/linux-imx-3.10.17/mx6/defconfig". But the linux kernel version is 3.14.28. Then how come the Yocto build uses the configuration file of linux kernel v3.10.17.
Please help me to understand this.
Appreciate your quick reply.
Thanks,
Dhaval
解決済! 解決策の投稿を見る。
Hi Khang,
I've started another post about this subject and described my work around for this on the following thread
Changing the Kernel configuration for i.MX6 SABRE
The only way I found to change my Kernel that works is to run the following commands in this particular order.
$ bitbake linux-imx -c cleansstate
$ bitbake linux-imx -c menuconfig
(change anything)
$ bitbake linux-imx
But this changes the ./tmp rather than ../source, so changes are easily lost.
Cheers
Chris
Hi,
I'm having the same problem. Could you sum up what commands you ran to change the kernel and then rebuild it please.
cheers
Chris
Hi,
I'm also having the same problems... would love a resolution on this issue.
Hi Khang,
I've started another post about this subject and described my work around for this on the following thread
Changing the Kernel configuration for i.MX6 SABRE
The only way I found to change my Kernel that works is to run the following commands in this particular order.
$ bitbake linux-imx -c cleansstate
$ bitbake linux-imx -c menuconfig
(change anything)
$ bitbake linux-imx
But this changes the ./tmp rather than ../source, so changes are easily lost.
Cheers
Chris
hi Chris,
I really appreciate the detail steps and analysis. Still I am facing issue.
After executing last step
$ bitbake linux-imx
How to pick up the latest configured changed into kernel. I guess `tmp/deploy/images/imx6qsabresd/` should get updated.
please guide.
Br,
kaustubh
Hi Kaustubh,
when you run the "-c cleansstate" you will find all of the files in tmp/deploy/images/imx6qsabresd/ are removed. Then by running "-c menuconfig" and building again it seems to regenerate all of these files with your kernel changes in.
This means you can use tmp/deploy/images/imx6qsabresd/core-image-base-imx6qsabresd.sdcard (eg for bitbake core_image_base) to program your sdcard.
After you boot up you can verify your kernel options by using (if CONFIG_IKCONFIG and CONFIG_IKCONFIG_PROC are set, but these seem to be disabled in the latest release, eg 3.14.38)
$ cat /proc/config.gz | gunzip
cheers
Chris
Thanks chris,
It worked !
It has updated uimage in tmp/deploy/images/../ folder.
modules-.xxx.tgz also got updated modules i think. So on board using SD card I am able to change kernel uImage.
Could you please tell where to copy on board these modules ?
br,
kdj
Hi kdj,
I'm a bit of a newbie as well. What are these modules-.xxx.tgz? I haven't seem them before, what are you trying to do?
If you look at Changing the Kernel configuration for i.MX6 SABRE you will see Surabh posted a comment with a link to a tutorial
https://community.freescale.com/servlet/JiveServlet/previewBody/95096-102-10-7847/yocto_tutorial.pdf
I'm planning to work through it next week. So hopefully I'll know more then. It might be worth posting all future comments to the other discussion.
cheers
Chris
Hi
Dhaval
You can select imx-3.14.28-1.0.0_ga
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga
Or you can use the
PREFERRED_VERSION_linux-imx_mx6 = "3.14.28"
Hi Saurabh,
Thanks for your quick reply!
Actually, I followed the Freescake Yocto Project User's Guide available in the documentation of "fsl-yocto-3.14.28-1.0.0". I sync the repo mentioned in that document. Now as you mentioned to sync with different repo. Then do I need to remove the old repo? It would be really great if you can elaborate the options you have suggested.
I want to know how to build the kernel again after changing it's configuration using Yocto.
Thanks,
Dhaval
Hi,
Can someone please help me here?
Thanks,
Dhaval
Hello Dhaval Vadhar,
Would you please confirm which repo were you using?
In case you switch repo you should just change the repo and run a sync. However, I would recommend using a new directory in case you will jump to a new kernel version.
There is a simple buy good document on how to change the kernel configuration on the following link, perhaps it will help.
Hi,
Thanks for your help!
As I said before, I was following Freescale Yocto Project User's Guide from 'fsl-yocto-3.14.28-1.0.0' documentation. Thus I have used following command to sync with the repo:
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga
$ repo sync
I also read the Yocto Training Task #5. According to that to change the kernel configuration I need to replace the 'defconfig' file from "meta-fsl-arm/receipes-kernel/linux/linux-imx-<kernel version>/mx6". Now in my case, the 'kernel version' should be '3.14.28', but that directory doesn't exist. Instead directory 'linux-imx-3.10.17/mx6' is exist.
Thus I am getting little confused, how to change the kernel configuration and then built it using 'bitbake linux-imx' command. Please help me for the same.
Appreciate your quick reply!
Thanks,
Dhaval
Hi
Dhaval
Please use following in local.conf to build 3.14.28 kernel.
PREFERRED_VERSION_linux-imx_mx6 = "3.14.28"
Thanks
Saurabh
Hi Saurabh,
Thanks for quick response!
I am able to build the linux kernel using 'bitbake linux-imx' command. But my question is how to build the kernel after changing the configuration?
Thanks,
Dhaval
Hi Saurabh,
Thanks once again for your reply!
That tutorial was really good. But it hasn't answered my question.
Thanks,
Dhaval
bitbake linux-imx -c menuconfig
linux-imx_3.14.28.bb
do_configure_prepend() {
# copy latest defconfig for imx_v7_defconfig to use
cp ${S}/arch/arm/configs/imx_v7_defconfig ${S}/.config
cp ${S}/arch/arm/configs/imx_v7_defconfig ${S}/../defconfig
fi
}
Hi Biyong,
Thanks for your reply!
As you suggested, I need to add the do_configure_prepend() function in linux-imx_3.14.28.bb file. But that file is not exist.
So do I need to create it? If yes, what else I need to add into that file?
Thanks,
Dhaval
linux-imx_3.14.28.bb is just take 3.14.28 release as example.
What is your BSP version?
Like 3.10.53, you can find
fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.53.bb
BSP Version is : 3.14.28
But the sources directory, sources/meta-fsl-arm/recipes-kernel/linux, doesn't have any directory/.bb file for linux version 3.14.28. Instead it has directory and .bb file for 3.10.17.
So do I need to create the .bb file for 3.14.28 manually?