Hi,
I am trying to compile kernel source ( rel_imx_4.1.15_1.1.0_ga) with imx_v6_v7_defconfig for my iMX6Q SABRE AI EVK. But I am getting the following error,
make -j4 uImage LOADADDR=0x10008000
.
.
.
LINK vmlinux
LD vmlinux.o
MODPOST vmlinux.o
GEN .version
CHK include/generated/compile.h
UPD include/generated/compile.h
CC init/version.o
LD init/built-in.o
drivers/built-in.o: In function `mxsfb_probe':
debugfs.c:(.text+0x459dc): undefined reference to `mxc_dispdrv_gethandle'
make: *** [vmlinux] Error 1
Please suggest the correct configuration for SABRE AI board.
My aim is to test hibernation (suspend-to-disk) on the same board with a gstreamer based audio/video Qt5 application, and i found that kernel 4.1.15 have support for the same. Has this been tried before? Is there any known issues with hibernation (supend-to-disk) on ARM?
Thanks and Regards,
Shyam
Hi jimmychan,
No, I got the rel_imx_4.1.15_1.1.0_ga kernel source code from freescale git and i am just running the commands
make imx_v6_v7-defconfig
make -j4 uImage LOADADDR=10008000
Note: imx_v7_defconfig seems working fine with imx6q sabre AI board
Thanks
shyam
Maybe I have a solution for you. It seems that the imx_v6_v7-defconfig has some incompatibilities.
At least I finished a compilation with attached .config-file. Would you give it a try?
Unfortunately the Kernel doesn't start completely. It seems to stuck after about 3 to 4 seconds at different states.