Jump to IMX boot rom SDP ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jump to IMX boot rom SDP ?

709 Views
SJA
Contributor II

Is there a way to jump from uboot into the boot rom USB SDP ?

Would like a fallback if uboot cannot boot the kernel.

I could use the sdp uboot command except that seems to allow
bypass of secure boot ... alternately is there a way to make the uboot sdp implementation secure ?


Currently working with imx6ull ....

0 Kudos
Reply
2 Replies

700 Views
b36401
NXP Employee
NXP Employee

There is no such option to jump. You should issue a reset to enter boot ROM again.

0 Kudos
Reply

703 Views
igorpadykov
NXP Employee
NXP Employee

Hi SJA

 

>jump from uboot into the boot rom USB SDP ?

>Would like a fallback if uboot cannot boot the kernel.

 

I am afraid this is not possible. In general one can try to use wdog, so it will reset

when uboot fail to boot kernel.

 

Best regards
igor

0 Kudos
Reply