Hi community.
IMX6 SABRE AI CPU Card, at the Revision B, when look at the circuit around JTAG CONNECTR of J17, JTAG_nTRST has not been connected to the J17.
(TRSTB terminal of iMX6 has H level is always input)
TRSTB terminal is the H level fixed, there is no problem?
已解决! 转到解答。
According to Table 2-19 (JTAG interface summary) of “Hardware Development
Guide for i.MX 6 …” :
JTAG_TRSTB input of i.MX6 has internal 47 kOhm pull up and
external pull up is not required; nevertheless it is possible to
apply external 10 kOhm pull up.
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takahashi
In addition to Yuri's explanations please also
note that JTAG_nTRST is an optional pin
for JTAG debugging and most JTAG debuggers
can work without this pin (and reset the TAP
with a different sequence).
Hope this helps
Regards
Sinan Akman
According to Table 2-19 (JTAG interface summary) of “Hardware Development
Guide for i.MX 6 …” :
JTAG_TRSTB input of i.MX6 has internal 47 kOhm pull up and
external pull up is not required; nevertheless it is possible to
apply external 10 kOhm pull up.
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------