JTAG Debugger for iMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Debugger for iMX6UL

1,090 Views
surendradhobale
Contributor III

Hello,

         We are looking to develop custom board using the iMX6UL controller ( ARM Cortex A7). We are planning to use Linux platform for same. In board bring up ( for DDR3 timing ) , develoment looking to use the JTAG debugger.

Which debugger is really compatible with iMX6UL.

Can you please provide the few name of the debugger, so that we can purchase ?

Regards,

Surendra

Labels (1)
Tags (1)
0 Kudos
1 Reply

609 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

one can look at AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK

describing some debuggers

http://www.nxp.com/assets/documents/data/en/application-notes/AN5229.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos