JTAG: CM7 DAP vs SJC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG: CM7 DAP vs SJC

Jump to solution
578 Views
spiderman
Contributor III

I am reading the application note AN12419 "Secure JTAG for i.MXRT10xx".

I understand there are two interfaces for debugging:

1) CM7 DAP

2) SJC

I understand that, if I want to use Secure JTAG mode, I must use SJC and permanently disable DAP by blowing fuses KTE=1 and SJC_MODE=01. Is this correct?

Also, apart from security, what are the differences and advantages/disadvantages of CM7 DAP vs SJC?

0 Kudos
1 Solution
539 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, SJC_SMODE needs to be b01 and KTE_FUSE burned after this one.
SJC is used for test like boundary scan, it is also used for Secure JTAG Challenge so after successfully executing this challenge the device is able to use CM7 DAP. So they both are completely different.
Please refer to chapters 3.1 and 4 from that application note.

Best regards,
Omar

View solution in original post

0 Kudos
1 Reply
540 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, SJC_SMODE needs to be b01 and KTE_FUSE burned after this one.
SJC is used for test like boundary scan, it is also used for Secure JTAG Challenge so after successfully executing this challenge the device is able to use CM7 DAP. So they both are completely different.
Please refer to chapters 3.1 and 4 from that application note.

Best regards,
Omar

0 Kudos