Dear experts,
I have a custom board with a Freescale iMX6 Solo CPU, and trying to use J-Link Commander to connect to the device.
I'm getting an error message, as seen in the log below.
Any ideas what might be the reason for this?
/////// Log Start /////
SEGGER J-Link Commander V4.90b ('?' for help)
Compiled Aug 14 2014 09:41:15
DLL version V4.90b, compiled Aug 14 2014 09:40:57
Firmware: J-Link Ultra V4 compiled Jul 28 2014 08:28:13
Hardware: V4.00
S/N: 504301229
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
VTarget = 3.116V
Info: TotalIRLen = 13, IRPrint = 0x0101
WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet=2)
Info: ARM AP[0]: 0x44770001, AHB-AP
Info: ARM AP[1]: 0x24770002, APB-AP
Info: Found Cortex-A9 r2p10
Info: 6 code breakpoints, 4 data breakpoints
Info: Debug architecture ARMv7.0
Info: Data endian: little
Info: Main ID register: 0x412FC09A
Info: L1 (I-cache): 32 KB, 256 sets, LineSize 32 bytes, 4-way
Info: L1 (D-cache): 32 KB, 256 sets, LineSize 32 bytes, 4-way
Info: System control register:
Info: Instruction endian: little
Info: Level-1 instruction cache enabled
Info: Level-1 data cache disabled
Info: MMU disabled
Info: Branch prediction disabled
Found 3 JTAG devices, Total IRLen = 13:
#0 Id: 0x4BA00477, IRLen: 04, IRPrint: 0x1, CoreSight JTAG-DP (ARM)
#1 Id: 0x00000001
#2 Id: 0x1891B01D
Cortex-A9 identified.
Target interface speed: 100 kHz
J-Link>r
Reset delay: 0 ms
Reset type NORMAL: Toggle reset pin and halt CPU core.
Info: Cortex-A/R (reset): Re-initializing debug logic.
WARNING: CPU not halted after Reset, halting using Halt request
****** Error: Bad JTAG communication: Write to IR: Expected 0x1, got 0xF (TAP Command : 10) @ Off 0x5.
//////// End //////////
Regards,
Erez
解決済! 解決策の投稿を見る。
I found that for iMX6, the device must be given to J-Link in the command line.
E.g.
JLINK.EXE -Device MCIMX6S1
Then, reset works fine.
I found that for iMX6, the device must be given to J-Link in the command line.
E.g.
JLINK.EXE -Device MCIMX6S1
Then, reset works fine.
Hi Erez
J-Link Commander is very simple tool designed just for testing J-Link,
for operation with i.MX6 seems one needs to use full-featured tools as
described below on segger forums:
SEGGER - The Embedded Experts - J-Link Commander
Getting J-Link working with i.MX6Q - J-Link/Flasher related - SEGGER Forum
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------