Hello,
I got an J-Link Base Adapter from Segger and I would like to check if the JTAG Interface on the IMX8QM is working. Is there some Documentation how to use a J-LINK Adapter on IMX8QM with such an Adapter?
Further I want to disable JTAG by fusing the fuses and verify if that operation truely disabled the JTAG Interface.
Best Regards,
Oliver
已解决! 转到解答。
I found that there is already a pending Patch for imx8qm config. Which is until now not on the mainline openocd.
http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg
Using that patch and with a few modifications in nxp_mcimx8m-evk.cfg it is working for me.
Best regards,
Oliver
Unfortunately I don't have access to the Lauterbach software.
I would like to the use the free and open source software "openocd" instead.
But until now there is no support for imx8qm. As far as I oversee this there is missing some board/target configuration files for imx8qm.
Is it possible that NXP can provide the necessary informations that we can try to implement this in openocd?
I found that there is already a pending Patch for imx8qm config. Which is until now not on the mainline openocd.
http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg
Using that patch and with a few modifications in nxp_mcimx8m-evk.cfg it is working for me.
Best regards,
Oliver
Hello,
For the i.MX8QM the JTAG debugger tested are:
Cortex-M -> Lauterbatch/J-LINK plus
Cortex-A -> Lauterbatch/DSStream
You may also refer to the following guide:
Normal and Secure Debug for i.MX8/8X Family of Applications Processors
Best regards,
Aldo.