It cann't be flashed to the target board by using the MFGTool.  

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

It cann't be flashed to the target board by using the MFGTool.  

1,534 Views
m7Cgde
Contributor I

Hello,

I have a MCIMX6SLEVK board.

It cann't be flashed to the target board by using the MFGTool.

The version is android_N7.1.2_2.0.0_image_6slevk.tar.gz which is download from NXP web.

The tool is android_N7.1.2_2.0.0_tools.tar.gz which is download from NXP web too.

All the steps are follow <<Android™ Quick Start Guide, Rev. N7.1.2_2.0.0, 10/2017>>.

when I Double-click the mfgtool2-android-mx6sl-evk-sd.vbs ,it didn't work.

The attachments show all the steps and also the log .

   Thanks

   AaronZ

Labels (1)
0 Kudos
Reply
2 Replies

1,404 Views
art
NXP Employee
NXP Employee

The logs you've provided show that the MFGtool software does not recognize the attached i.MX6 hardware for some reason. Most likely, the i.MX BulkIO driver is not installed correctly. Try to re-install it first.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,404 Views
m7Cgde
Contributor I

This issue has been resolved.

I have to change a laptop.

Use windows7 ,32bit. The MfgTool works good.

0 Kudos
Reply