I am currently trying to get Android 5.1.1 to boot up on a imx6 platform (solidrun i2ex SoM) by following the most recent guide from NXP. I have a 800x480 7" LCD connected via a parallel RGB interface and can see the initial Android logo but never get to the home screen. I have attached the bootup log showing in logcat where it appears some errors occur with SurfaceFlinger towards the very end of the log. Any assistance or suggestions would be greatly appreciated!
Original Attachment has been moved to: log_cubox_env_setup.log.zip
Hi David
NXP BSPs support only NXP boards: Sabre SD, AI. For other boards
customization should be implemented by vendors of these boards.
It may be suggested to start porting this board with linux uboot logo,
for example below examples for various LCDs:
https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
Then port other drivers using attached Porting Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------