Issues with Android 5.1.1 on imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with Android 5.1.1 on imx6

681件の閲覧回数
davidwebster
Contributor I

I am currently trying to get Android 5.1.1 to boot up on a imx6 platform (solidrun i2ex SoM) by following the most recent guide from NXP.  I have a 800x480  7" LCD connected via a parallel RGB interface and can see the initial Android logo but never get to the home screen. I have attached the bootup log showing in logcat where it appears some errors occur with SurfaceFlinger towards the very end of the log.  Any assistance or suggestions would be greatly appreciated!

Original Attachment has been moved to: log_cubox_env_setup.log.zip

ラベル(4)
0 件の賞賛
返信
1 返信

427件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi David

NXP BSPs support only NXP boards: Sabre SD, AI. For other boards

customization should be implemented by vendors of these boards.

It may be suggested to start porting this board with linux uboot logo,

for example below examples for various LCDs:

https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

Then port other drivers using attached Porting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信