Issue with MIPI-CSI0 4-lane by AR0144+AP1302 on I.MX8ULP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with MIPI-CSI0 4-lane by AR0144+AP1302 on I.MX8ULP

1,250 Views
yanger_yang
Contributor I

Hi All,

We use our camera(AR0144+AP1302) on i.mx8ulp-evk.

We can put the camera on CSI0 (/dev/video0), but can't use GStreamer to output video on screen.

 

root@imx8ulpevk:~# gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=1280,height=800 ! waylandsink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[   55.136111] bypass csc
[   55.138561] input fmt YUV4
[   55.141314] output fmt YUYV

 

Here is our .dts and the graph obtained from media-ctl --print-dot and v4l2-ctl --list-devices.

 

root@imx8ulpevk:~# media-ctl -p
Media controller API version 5.10.72

Media device information
------------------------
driver          mxc-md
model           FSL Capture Media Device
serial          
bus info        
hw revision     0x0
driver version  5.10.72

Device topology
- entity 1: mxc_isi.0 (16 pads, 2 links)
            type V4L2 subdev subtype Unknown flags 0
	pad0: Sink
		<- "mxc-mipi-csi2.0":4 [ENABLED]
	pad1: Sink
	pad2: Sink
	pad3: Sink
	pad4: Sink
	pad5: Sink
	pad6: Sink
	pad7: Sink
	pad8: Sink
	pad9: Sink
	pad10: Sink
	pad11: Sink
	pad12: Source
		-> "mxc_isi.0.capture":0 [ENABLED]
	pad13: Source
	pad14: Source
	pad15: Sink

- entity 18: mxc_isi.0.capture (1 pad, 1 link)
             type Node subtype V4L flags 0
             device node name /dev/video0
	pad0: Sink
		<- "mxc_isi.0":12 [ENABLED]

- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)
             type Node subtype V4L flags 0
             device node name /dev/v4l-subdev0
	pad0: Sink
		<- "tevi-ap1302 0-003d":0 [ENABLED,IMMUTABLE]
	pad1: Sink
	pad2: Sink
	pad3: Sink
	pad4: Source
		-> "mxc_isi.0":0 [ENABLED]
	pad5: Source
	pad6: Source
	pad7: Source

- entity 31: tevi-ap1302 0-003d (1 pad, 1 link)
             type V4L2 subdev subtype Sensor flags 0
	pad0: Source
		-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]

 

 

root@imx8ulpevk:~# v4l2-ctl --list-devices
mxc-isi-cap (platform:2dac0000.isi:cap_devic):
/dev/video0

FSL Capture Media Device (platform:mxc-md):
/dev/media0

root@imx8ulpevk:~#

 

 

#include "imx8ulp-evk.dts"

&i2c_rpbus_0 {
	/delete-node/ ov5640_mipi@3c;

	ap1302_otp_0: eeprom@54 {
		compatible = "atmel,24c1024";
		reg = <0x54>;
		pagesize = <128>;
		//read-only;
	};

	tevi_ap1302_mipi@3d {
		compatible = "tn,tevi-ap1302";
		reg = <0x3d>;

		standby-gpios = <&pca6416_1 8 GPIO_ACTIVE_HIGH>;
		reset-gpios = <&pca6416_1 7 GPIO_ACTIVE_HIGH>;

		nvmem = <&ap1302_otp_0>;
		nvmem-names = "calib-data";
		status = "okay";

		port {
			ap1302_mipi_0_ep: endpoint {
				remote-endpoint = <&mipi_csi0_ep>;
				data-lanes = <4>;
			};
		};
	};
};

&mipi_csi0 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";

	port@0 {
		reg = <0>;
		mipi_csi0_ep: endpoint {
			remote-endpoint = <&ap1302_mipi_0_ep>;
			data-lanes = <4>;
			bus-type = <4>;
		};
	};
};

 

Try to use data-lanes = <1 2>; the image can be output video, but the picture is abnormal.

IMG_4563.jpg

Are there any other configuration setting on MIPI-CSI0 when use 4 lanes?

The driver works fine on i.mx8mp-evk and i.mx8mn-evk boards.

Thanks a lot.

0 Kudos
3 Replies

780 Views
udhayamoorthi
Contributor II

@yanger_yang 

how you are interfacing ar0144 and ap1302?

 in .dts you are mention only ap1302 so how ar0144 is configured?

0 Kudos

1,221 Views
yanger_yang
Contributor I

Hello everyone,

I checked the reference specification of i.mx8upl, it states that MIPI-SCI only supports 2 lanes at most, therefore I changed the setting to 2 lanes, but the video output screen is still not normal, as follows:

unnamed (1).jpg

0 Kudos

1,201 Views
jimmychan
NXP TechSupport
NXP TechSupport

8ULP DPHY only support up to 2 data lanes, so customer must use new 2 lane ap1302 firmware on 8ULP.

0 Kudos