Issue using VPU on imx6qp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue using VPU on imx6qp

1,262 Views
stuartmorton
Contributor II

Hi,

I'm trying to play a video using gstreamer but i think there is an issue with the VPU. Here is what i have tried:

as a test, running the following works as expected:

gst-launch-1.0 videotestsrc ! imxipuvideosink

Next i tried running :

gst-launch-1.0 playbin uri=file:///home/root/small.mp4

which gives:

...

[ERR] Error in opening firmware binary file
[ERR] Please put bin file to /lib/firmware/vpu folder or export VPU_FW_PATH env

...

I have an imx-vpu recipe in my build which generates an imx-vpu-5.4.35.bin. As far as I'm aware, this is the firmware gstreamer needs. It isn't copied automatically but manually naming it vpu_fw_imx6q.bin and moving into /lib/firmware/vpu removes the given error. running the playbin command again now gives:

EDIT: the imx-vpu-5.4.35.bin was not the right file and is used for something else. I have since tried multiple firmware files but i still get the same results.

Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...

====== AIUR: 4.1.4 build on Sep 25 2017 17:00:54. ======
    Core: MPEG4PARSER_06.09.36  build on Aug 23 2016 05:18:47
 file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2
------------------------
    Track 00 [video_0] Enabled
    Duration: 0:00:05.533333000
    Language: und
    Mime:
    video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)560, height=(int)320, framerate=(fraction)30/1, codec_data=(buffer)0142c01effe1001b6742c01e9e218118534d40404050000003001000000303c8f162ee01000568ce06cb20
------------------------
------------------------
    Track 01 [audio_0] Enabled
    Duration: 0:00:05.568000000
    Language: eng
    Mime:
    audio/mpeg, mpegversion=(int)4, channels=(int)1, rate=(int)48000, bitrate=(int)83051, stream-format=(string)raw, codec_data=(buffer)1188
------------------------
display(/dev/fb0) resolution is (1024x600).
====== OVERLAYSINK: 4.1.4 build on Sep 25 2017 17:01:05. ======
display(/dev/fb0) resolution is (1024x600).

====== BEEP: 4.1.4 build on Sep 25 2017 17:00:57. ======
    Core: AAC decoder Wrapper  build on May 30 2016 12:33:44
 file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm12_elinux.so.3
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_CORTEX-A8  build on Jul 13 2016 18:15:25.

At this point nothing happens (hangs with no output) and continues to do nothing until interrupted.

I tried running the decode examples from GitHub - Freescale/libimxvpuapi: i.MX VPU API Library  and it seems to hang on vpu_init. Using VPU debug output gives:

$ ./mxc_vpu_test.out -D "-i /unit_tests/akiyo.mp4 -f 2 -t 1 -a 60 -y 1"

[INFO]    VPU test program built on Sep 26 2017 13:48:22
[DEBUG]    vpu_lib.c:274 enter vpu_Init()
[DEBUG]    vpu_io.c:99 kernel:4.1.15-gb7c1e35-dirty, 4.1.15
[DEBUG]    vpu_io.c:165 soc: i.MX6Q, rev: 0x63012
[DEBUG]    vpu_util.c:1352 sema not init
[DEBUG]    vpu_util.c:1379 sema inited
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 1
[DEBUG]    vpu_io.c:537 _IOGetPhyMem: phy addr = 6a100000
[DEBUG]    vpu_io.c:538 _IOGetPhyMem: alloc=507904, total=507904
[DEBUG]    vpu_io.c:724 IOGetVirtMem: virt addr = 76516000
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 0
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 1
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 1
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 0
[DEBUG]    vpu_io.c:811 vpu clock gate setting = 1

Then waits indefinitely like before.

Testing this on an imx6q (not a plus) gave similar results.

Any help would be appreciated.

Thanks

Labels (2)
Tags (2)
0 Kudos
1 Reply

676 Views
joanxie
NXP TechSupport
NXP TechSupport

what yocto version do you use? I built 4.1.15 on mx6q board, and use mxc_vpu_test and gstreamer successfully, how could I reproduce your issue?

0 Kudos