Issue in reading more than 28 bytes using spidev for iMX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in reading more than 28 bytes using spidev for iMX7D

1,402 Views
anoop2
Contributor II

Hello

I'm using iMX7D based board and trying to interface a device over SPI using a custom data exchange protocol. On the Host side, I'm using spidev to implement SPI Master functionality. I created a SPI node for ECSPI3 in DTB file and verified that /dev/spidevX.0 is created on Host. I'm using https://github.com/azorg/spi as a reference to create Host side code.

The communication with SPI slave device is configured to use SPI_MODE_1 at 10Mhz clock frequency. I can read and write up to 28 bytes without any issue. But when I try to use data transfer larger than 28 bytes, it fails (It actually transfers just 1 or 2 bytes).

To further isolate the issue, I've tested the same SPI slave device with the same Host side code running on a Raspberry Pi. With Raspberry Pi, I'm able to read and write more than 28 bytes without any issue.

So this seems an issue with the way SPI Master device is configured on iMX7. Could you please help me to solve or further debug this issue.

Thanks

0 Kudos
Reply
1 Reply

1,390 Views
anoop2
Contributor II

It was an issue related to configuration in DTB file. The issue is solved now.

 

Tags (1)