Issue in DDR calibration values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue in DDR calibration values

570 次查看
hrushinale
Contributor III

Hello Community,

We have two variants of custom board first one based on i.MX6 solo with 1GB ram and another based on i.MX6 Dualite with 2GB RAM.

When I run the DDR calibration for dualite board I got 12 updated calibration values

but when I run the calibration for Solo board with 1GB ,I am getting only 4 updated calibration values.

So my question is How can I get all the 12 calibration values for solo board?

we followed I.MX6DQSDL DDR3 Script Aid V0.10 .

Thanks & Regards,

Hrushi

标记 (3)
0 项奖励
回复
2 回复数

462 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

seems this is described in sect.3.3.1 Identifying Issue on Calibrations

MX6 DRAM Port Application Guide :

There is a chance that there is an error during the calibration, it may

fail to find a valid delay window for some particular bytes.

Freescale i.MX6 DRAM Port Application Guide-DDR3 | NXP Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

462 次查看
hrushinale
Contributor III

Hello Igorpadykov,

I run the test multiple times on two different solo boards but still I am getting only four values and not 12.

Kindly guide us regarding this issue.

Thanks & Regards,

Hrushi

0 项奖励
回复