Is there any way that I still can get this BSP android_jb4.2.2_1.0.0-ga.tar.gz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way that I still can get this BSP android_jb4.2.2_1.0.0-ga.tar.gz?

ソリューションへジャンプ
3,541件の閲覧回数
tzeyeelau
Contributor I

I tried to download JB4.2.2_1.0.0 Release from this link https://community.freescale.com/docs/DOC-94798# but failed to get it for some reason.

Is there any place that I still can get this release?

Thank you.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,070件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may try the link, I have sent You.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
2,070件の閲覧回数
sachingarg2k1
Contributor I

Hi Yuri,

Can you send me the link to download JB4.2.2_1.0.0 release.

Thanks,

Sachin

0 件の賞賛
返信
2,070件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
2,071件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may try the link, I have sent You.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,070件の閲覧回数
tzeyeelau
Contributor I

Yuri, many thanks to you.

Do you mind that I share your link to Saurabh?

0 件の賞賛
返信
2,070件の閲覧回数
Yuri
NXP Employee
NXP Employee

yes, why not ?

0 件の賞賛
返信
2,070件の閲覧回数
tvkai
Contributor I

Hi Yuri, Have a good day. I'm new here

My project requires jb4.2.2 only. Would you mind sending me the source download link too?

Thanks & Regards

Kai

0 件の賞賛
返信
2,070件の閲覧回数
Yuri
NXP Employee
NXP Employee

The "android_jb4.2.2_1.1.0-ga_source" is not located on the Web more.

You may try to download it via my Google disk :

< https://drive.google.com/file/d/0B0qEfizitWXlSk1JM0d6RnV5S2M/edit?usp=sharing >

Regards,

Yuri.

0 件の賞賛
返信
2,070件の閲覧回数
saurabh206
Senior Contributor III

Hi Yuri

Can you share the link to me also?

Thanks

Saurabh

0 件の賞賛
返信
2,070件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi TZE

you can enter ticket and get link from internal server,

then contact local FAE for obtaining access.

Best regards

igor

0 件の賞賛
返信
2,070件の閲覧回数
elvisdowson
Contributor I

Hi Igor,

I too require the source and binary demo images for Android-4.2.2 for the SABRE SDP platform.

The links mentioned in this document do not work for some reason: i.MX6 D/Q and i.MX6 DL/S Android JB4.2.2_1.0.0-GA release

Thanks!

Regards,

Elvis Dowson

0 件の賞賛
返信
2,070件の閲覧回数
saurabh206
Senior Contributor III

This is not working for some reason.

If you possible you can start working with JB4.3 or JB4.4.

Thanks

Saurabh

0 件の賞賛
返信
2,070件の閲覧回数
tzeyeelau
Contributor I

Many thanks for reply.

Our customer insists to use JB4.2.2, no matter how hard we asked them to switch to any version.

0 件の賞賛
返信