Is there a recommended PMIC for use with the i.MX 6ULL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a recommended PMIC for use with the i.MX 6ULL?

395 Views
dcade
Contributor I

I see the PF3001 is recommended for use with the 6UL but no mention of the 6ULL?

0 Kudos
1 Reply

343 Views
igorpadykov
NXP Employee
NXP Employee

Hi

6ULL is reduced version of 6UL, so the same pmic can be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos