Is there a documentation of Android M bsp development ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a documentation of Android M bsp development ?

815 Views
ganyeking
Contributor II

hi community:

Recently,i should fit android M driver for my custon-board ,it's relay on imx6q .Then,Does NXP provide like Androind M bsp development of technical documentation?

Best Regards

ganye

Labels (4)
0 Kudos
4 Replies

539 Views
igorpadykov
NXP Employee
NXP Employee

Hi ganye

specific i.MX documentation is included in android doc bundle

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.1.0_ANDROID_DOCS&Parent_nodeId=133769948107... 

there is no general android porting guide, one can refer to common android developers resources.

As android is based on linux, it may be useful to check linux porting guide included in

linux doc bundle

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

539 Views
ganyeking
Contributor II

Hi igor

Thank you for your prompt reply.Now ,I would like to learn more about Android M driver development, what book do you have any recommend books for me?

Thank you in advance.

Best Regards

ganye

0 Kudos

539 Views
ganyeking
Contributor II

Hi igor

Thank you very much.

Best Regards

ganye

0 Kudos