Is there a bare-metal reference code for iMX7 CAAM AES?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a bare-metal reference code for iMX7 CAAM AES?

622 Views
danielhu
Contributor I

It seems to me the only reference for bare metal on CAAM crypto accelerator is u-boot, which contain hash (sha1 and sha256) and rsa, but there is no support for symmetric operation like AES. Where could I find such example code?

the Kernel does have all stuff, but it has a far more complicated code base than u-boot, and it is not meant for bare-metal environment. 

0 Kudos
Reply
1 Reply

452 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

I am afraid such codes are not available.
Sorry for the inconvenience.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply